This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28062F: 修改ADC中断优先级

Part Number: TMS320F28062F


我想同时使用CAN和ADC中断,根据手册CAN中断位于第9组PIE,即INT9.5,电机控制例程的ADC中断位于10组,即INT10.1,这样的话CAN中断会打断ADC中断的执行,影响控制效果,我现在把ADC中断修改为INT1.1,发现还是有先CAN中断执行,请问一下可能是哪里的问题?

interrupt void WL_CAN_RX_ISR(void)
{

 //   HAL_acqEcanInt(halHandle);
    WEILANCANRx();
    HAL_acqEcanInt(halHandle);
}

//CAN接收函数
static inline void HAL_acqEcanInt(HAL_Handle handle)
{
    HAL_Obj *obj = (HAL_Obj *)handle;
    Ecan_clearIntFlag(obj->canHandle);
    PIE_clearInt(obj->pieHandle,PIE_GroupNumber_9);
}

static inline void Ecan_clearIntFlag(CAN_Handle canHandle)
{
  CAN_Obj *can = (CAN_Obj *)canHandle;


  // clear the bit
  can->ECanaRegs.CANRMP.all = 0xFFFFFFFF;

 return;
} // end of ADC_clearIntFlag() function