Original question:
UCD3138: Code Composer Studio 论坛
用的官方全程LLC_HB
编译平台为:Code Composer Studio 10.0.0
编译器为:TL v5.29
下载程序软件:UCD3xxx & UCD9xxx Device GUI
编译结果也没有告错,下载程序到芯片flash也正常(连续下载了两次也没有问题),运行程序功能也很正常;
但是断电后重新刷程序,就下载不了,为什么会这样? 怎么解决?
Hi
感谢您对TI产品的关注!关于UCD3138锁定或无法再烧录的问题,请参考下面两个资料:
https://www.ti.com/cn/lit/an/zhca646/zhca646.pdf
www.ti.com.cn/.../zhcacu3.pdf
我现在按照文档中的说明,用通信的方式执行pmbus_write_rom_mode()函数,但是只是清除了密码,但是在锁住的情况下,仍然无法解锁,为什么
提示如下
Error:Device does not appear to be in ROM mode after ENABLE_ROM_MODE command;after3154msec the ROM is still not responding
也可以尝试参考下面链接:
UCD3138: UCD3138 locked problem