Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, LAUNCHXL-F280039C, LAUNCHXL-F280025C, LAUNCHXL-F2800137, BOOSTXL-DRV8323RS
想使用的FAST软件编码的无传感器FOC解决方案实现零速获取初始位置,所以想问FAST算法库如何调用
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, LAUNCHXL-F280039C, LAUNCHXL-F280025C, LAUNCHXL-F2800137, BOOSTXL-DRV8323RS
想使用的FAST软件编码的无传感器FOC解决方案实现零速获取初始位置,所以想问FAST算法库如何调用
您好,
我没有在该文档中看到28379D应用InstaSPIN-FOC的相关介绍,只有以下三种芯片,C:\ti\c2000\C2000Ware_MotorControl_SDK_5_02_00_00\solutions\universal_motorcontrol_lab文件夹中只有f28002x、f28003x、、f280013x、f280015x,没有28379D,请问哪里有28379D的lab?
3.3.1 Importing and Configuring Project
The example lab is a universal project that has support for various TI EVM motor driver kits that can be used
in conjunction with the F280025C, F280039C, or F2800137 C2000 MCU devices. The user can run different
TI EVM kits by setting the build configurations and properties of the lab project. In the following sections,
the LAUNCHXL-F280025C, LAUNCHXL-F280039C, or LAUNCHXL-F2800137 is used in combination with the
BOOSTXL-DRV8323RS lab to show how to import and run the example lab on this kit.
1. Import the project within CCS by clicking "Project" ➔"Import CCS Projects...", and then click "Browse..."
button to select search directory at:
a. F28002x based
lab:<install_location>\solutions\universal_motorcontrol_lab\f28002x\ccs\motor_
control\ to select the "universal_motorcontrol_lab_f28002x" project.
b. F28003x based
lab:<install_location>\solutions\universal_motorcontrol_lab\f28003x\ccs\motor_
control\ to select the "universal_motorcontrol_lab_f28003x" project.
c. F280013x based
lab:<install_location>\solutions\universal_motorcontrol_lab\f280013x\ccs\motor
_control\ to select the "universal_motorcontrol_lab_f280013x" project.