Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: DRV8301, MOTORWARE
具体需求如下:
电机参数:一对磁极的三相无刷电机,电机的最大空载转速为60000±10% rpm。
具体要求:需控制电机在 100-50000rpm 顺畅运转,且速度误差不超过 2%,启动过程以及调速切换电机无明显抖动及卡顿现象;
实现扭力的精准控制,电机扭力范围内误差不超过5%。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
这里没有列出很多马达参数。 我相信您的要求是可以实现的,前提是: