This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一个问题,包是我写的基于TMS570ls12x的launchpad的一个简单的can发送

Other Parts Discussed in Thread: HALCOGEN

请教一个问题,包是我写的基于TMS570ls12x的launchpad的一个简单的can1发送,在资料查明can1的RX和TX分别是J10的38和39孔,我用杜邦线与CANalyst-Ⅱ相连,如何用USB_CAN TOOL查看接收的数据,发现并没有预想的数据发送过来,请教各位大神帮我分析一下原因,谢谢~

自己尝试测试,分析仪没有问题,分析仪与USB_CAN TOOL连接也没有问题,请各位大神赐教test_can.rar

  • TMS570ls12x是有相关的CAN通信例程的,您可以参考下

    /** @example example_canCommunication.c
    *   This is an example which describes the steps to create an example application which 
    *   configures two can nodes 1 and 2 and starts a communication with a sample data chunk.
    *   CAN 1 and CAN2 must be part of CAN network
    *
    *   
    *   @b Step @b 1:
    *
    *   Create a new project.
    *
    *   Navigate: -> File -> New -> Project
    *
    *   @image html example_createProject.jpg "Figure: Create a new Project"
    *
    *   @b Step @b 2:
    *
    *   Configure driver code generation: 
    *   - Enable can driver   
    *   - Disable others
    *
    *   Navigate: -> TMS570LSxx /RM4 -> Enable Drivers
    *
    *   @image html can_enabledriver.JPG "Figure: Enable CAN Driver"
    *
    *   @b Step @b 3:
    *
    *   Configure CAN Baudrate: 
    *
    *   Navigate: -> TMS570LSxx /RM4 -> CAN
    *
    *   @image html can1baud.JPG "Figure: CAN1 BaudRate Configuration"
    *   @image html can2baud.JPG "Figure: CAN2 BaudRate Configuration"
    *
    *   @b Step @b 4:
    *
    *   Configure CAN MessageBox: 
    *
    *   - Configure CAN1 , MessageBox 1 -- Activate and Enable TX
    *   - Configure CAN2 , MessageBox 1 -- Activate and Enable RX
    *
    *   Navigate: -> TMS570LSxx /RM4 -> CAN
    *
    *   @image html canCommunication1.JPG "Figure: CAN1 MBox Configuration"
    *   @image html canCommunication2.JPG "Figure: CAN2 MBox Configuration"
    *
    *   @b Step @b 5:
    *
    *   Copy the source code below into your sys_main.c or replace sys_main.c with this file.
    *
    *   The example file can also be found in the examples folder: ../HALCoGen/examples
    *
    *   @note HALCoGen generates an empty main function in sys_main.c, 
    *
    */
    
    /* 
    * Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com
    * 
    * 
    *  Redistribution and use in source and binary forms, with or without 
    *  modification, are permitted provided that the following conditions 
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright 
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the 
    *    documentation and/or other materials provided with the   
    *    distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES INCLUDING, BUT NOT 
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    *  INCLUDING NEGLIGENCE OR OTHERWISE ARISING IN ANY WAY OUT OF THE USE 
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    */
    
    /* USER CODE BEGIN (0) */
    /* USER CODE END */
    
    /* Include Files */
    
    #include "sys_common.h"
    #include "system.h"
    
    /* USER CODE BEGIN (1) */
    #include "can.h"
    
    /* Include ESM header file - types, definitions and function declarations for system driver */
    #include "esm.h"
    
    #define  D_SIZE 9
    
    uint8  tx_data[D_SIZE]  = {'H','E','R','C','U','L','E','S','\0'};
    uint8  rx_data[D_SIZE] = {0};
    uint32 error = 0;
    
    uint32 checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize);
    /* USER CODE END */
    
    
    /** @fn void main(void)
    *   @brief Application main function
    *
    */
    
    /* USER CODE BEGIN (2) */
    /* USER CODE END */
    
    
    void main(void)
    {
    /* USER CODE BEGIN (3) */
    
        /* initialize can 1 and 2   */
        canInit(); /* can1 -> can2 */                                      
    
        /* transmit on can1 */
        canTransmit(canREG1, canMESSAGE_BOX1, tx_data); 
    
        /*... wait until message receive on can2 */
        while(!canIsRxMessageArrived(canREG2, canMESSAGE_BOX1));
        canGetData(canREG2, canMESSAGE_BOX1, rx_data);  /* receive on can2  */
    
        /* check received data patterns */
        error = checkPackets(&tx_data[0],&rx_data[0],D_SIZE);
    
        /* ... run forever */
        while(1);
    
    /* USER CODE END */	
    }
    
    /* USER CODE BEGIN (4) */
    /** @fn checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize)
    *   @brief check two buffers and report error
    *
    */
    uint32 checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize)
    {
       uint32 err=0;
       uint32 cnt=psize;
    
       while(cnt--)
       {
         if((*src_packet++) != (*dst_packet++))
         {
            err++;           /*  data error  */
         }
       }
       return (err);
    }
    /* USER CODE END */

  • /** @example example_canIntCommunication.c
    *   This example code configures two CAN nodes and emulates a data transfer
    *   from CAN1 to CAN2.
    * 
    *   node1: CAN1 [MSG BOX 1 (ID1)]-> TX
    *   node2: CAN2 [MSG BOX 1 (ID1)]<- RX
    *   
    *   @b Step @b 1:
    *
    *   Create a new project.
    *
    *   Navigate: -> File -> New -> Project
    *
    *   @image html example_createProject.jpg "Figure: Create a new Project"
    *
    *   @b Step @b 2:
    *
    *   Configure driver code generation: 
    *   - Enable CAN driver
    *   - Disable others
    *
    *   Navigate: -> TMS570LSxx /RM4 -> Enable Drivers
    *
    *   @image html can_enabledriver.jpg "Figure: CAN 1,2 Driver Enable"
    *
    *   @b Step @b 3:
    *
    *   Configure CAN Message Box: 
    *   - Configure CAN1 Message box 1 as transmit
    *   Navigate: -> TMS570LSxx /RM4 -> CAN
    *
    *   @image html can1box.jpg "Figure: CAN1 MBox Configuration"
    *
    *   - Configure CAN2 Message box 1 as receive
    *
    *   @image html can2box.jpg "Figure: CAN2 MBox Configuration"
    *
    *   - Enable CAN1 High level interrupt and CAN2 High level interrupt  
    *
    *   @b Step @b 4:
    *
    *   Enable CAN interrupts in VIM: 
    *
    *   Navigate: -> TMS570LSxx /RM4 -> VIM
    *
    *   @image html can1_Int.jpg "Figure: VIM Configuration"
    *   @image html can2_Int.jpg "Figure: VIM Configuration"
    *
    *   @b Step @b 5:
    *
    *   Copy the source code below into your sys_main.c (or) replace sys_main.c with this file.
    *   Copy dma.c and dma.h into your application.
    *
    *   Execution:
    *   The CAN1 and CAN2 communication line needs to be connected on to the live CAN bus.
    * 
    *   The example file can also be found in the examples folder: ../HALCoGen/examples
    *
    *   @note HALCoGen generates an enpty main function in sys_main.c. 
    *
    */
    
    /* 
    * Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com
    * 
    * 
    *  Redistribution and use in source and binary forms, with or without 
    *  modification, are permitted provided that the following conditions 
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright 
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the 
    *    documentation and/or other materials provided with the   
    *    distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES INCLUDING, BUT NOT 
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    *  INCLUDING NEGLIGENCE OR OTHERWISE ARISING IN ANY WAY OUT OF THE USE 
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    */
    
    /* USER CODE BEGIN (0) */
    /* USER CODE END */
    
    /* Include Files */
    
    #include "sys_common.h"
    #include "system.h"
    
    /* USER CODE BEGIN (1) */
    #include "can.h"
    #include "esm.h"
    #include "sys_core.h"
    
    #define D_COUNT  8 
    
    uint32 cnt=0, error =0, tx_done =0;
    uint8 tx_data[D_COUNT][8] = {0};
    uint8 rx_data[D_COUNT][8] = {0};
    uint8 *tx_ptr = &tx_data[0][0];
    uint8 *rx_ptr = &rx_data[0][0];
    uint8 *dptr=0;
    
    void dumpSomeData();
    /* USER CODE END */
    
    
    /** @fn void main(void)
    *   @brief Application main function
    *
    */
    
    /* USER CODE BEGIN (2) */
    /* USER CODE END */
    
    
    void main(void)
    {
    /* USER CODE BEGIN (3) */
    
        /* enable irq interrupt in Cortex R4 */
        _enable_interrupt_();
    
        /** - writing a random data in RAM - to transmit */
        dumpSomeData();
            
        /** - configuring CAN1 MB1,Msg ID-1 to transmit and CAN2 MB1 to receive */
        canInit();
    
        /** - enabling error interrupts */    
        canEnableErrorNotification(canREG1);
    	canEnableErrorNotification(canREG2);
        
        /** - starting transmission */
         for(cnt=0;cnt<D_COUNT;cnt++)
        {         
          canTransmit(canREG1, canMESSAGE_BOX1, tx_ptr); /* transmitting 8 different chunks 1 by 1 */
          while(tx_done == 0){};                 /* ... wait until transmit request is through        */
          tx_done=0;
          tx_ptr +=8;    /* next chunk ...*/
        }
        
        /** - check the received data with the one that was transmitted */
        tx_ptr = &tx_data[0][0];
        rx_ptr = &rx_data[0][0];
            
        for(cnt=0;cnt<63;cnt++)
         {
              if(*tx_ptr++ != *rx_ptr++)
              {
                   error++; /* data error */
              }
         }
    
        while(1){}; /* wait forever after tx-rx complete. */
    	
    /* USER CODE END */	
    }
    
    /* USER CODE BEGIN (4) */
    /* writing some data to ram  */
    void dumpSomeData()
    {
         uint32 tmp = 0x11;
         
         cnt = (D_COUNT*8)-1;
         dptr = &tx_data[0][0];
         *dptr = tmp;
    
         while(cnt--)
         {
            tmp = *dptr++;
            *dptr = tmp + 0x11;
         }
    }
    
    
    /* can interrupt notification */
    /* Note-You need to remove canMessageNotification from notification.c to avoid redefinition */
    void canMessageNotification(canBASE_t *node, uint32 messageBox)
    {
         /* node 1 - transfer request */
         if(node==canREG1) 
         {     
           tx_done=1; /* confirm transfer request */
         }
    
         /* node 2 - receive complete */     
         if(node==canREG2)
         {
          while(!canIsRxMessageArrived(canREG2, canMESSAGE_BOX1));
          canGetData(canREG2, canMESSAGE_BOX1, rx_ptr); /* copy to RAM */    
          rx_ptr +=8;     
         }     
    
        /* Note: since only message box 1 is used on both nodes we dont check it here.*/
    }
    /* USER CODE END */

    /** @example example_canIntCommunication.c*   This example code configures two CAN nodes and emulates a data transfer*   from CAN1 to CAN2.* *   node1: CAN1 [MSG BOX 1 (ID1)]-> TX*   node2: CAN2 [MSG BOX 1 (ID1)]<- RX*   *   @b Step @b 1:**   Create a new project.**   Navigate: -> File -> New -> Project**   @image html example_createProject.jpg "Figure: Create a new Project"**   @b Step @b 2:**   Configure driver code generation: *   - Enable CAN driver*   - Disable others**   Navigate: -> TMS570LSxx /RM4 -> Enable Drivers**   @image html can_enabledriver.jpg "Figure: CAN 1,2 Driver Enable"**   @b Step @b 3:**   Configure CAN Message Box: *   - Configure CAN1 Message box 1 as transmit*   Navigate: -> TMS570LSxx /RM4 -> CAN**   @image html can1box.jpg "Figure: CAN1 MBox Configuration"**   - Configure CAN2 Message box 1 as receive**   @image html can2box.jpg "Figure: CAN2 MBox Configuration"**   - Enable CAN1 High level interrupt and CAN2 High level interrupt  **   @b Step @b 4:**   Enable CAN interrupts in VIM: **   Navigate: -> TMS570LSxx /RM4 -> VIM**   @image html can1_Int.jpg "Figure: VIM Configuration"*   @image html can2_Int.jpg "Figure: VIM Configuration"**   @b Step @b 5:**   Copy the source code below into your sys_main.c (or) replace sys_main.c with this file.*   Copy dma.c and dma.h into your application.**   Execution:*   The CAN1 and CAN2 communication line needs to be connected on to the live CAN bus.* *   The example file can also be found in the examples folder: ../HALCoGen/examples**   @note HALCoGen generates an enpty main function in sys_main.c. **/
    /* * Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com* * *  Redistribution and use in source and binary forms, with or without *  modification, are permitted provided that the following conditions *  are met:**    Redistributions of source code must retain the above copyright *    notice, this list of conditions and the following disclaimer.**    Redistributions in binary form must reproduce the above copyright*    notice, this list of conditions and the following disclaimer in the *    documentation and/or other materials provided with the   *    distribution.**    Neither the name of Texas Instruments Incorporated nor the names of*    its contributors may be used to endorse or promote products derived*    from this software without specific prior written permission.**  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES INCLUDING, BUT NOT *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION HOWEVER CAUSED AND ON ANY*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT *  INCLUDING NEGLIGENCE OR OTHERWISE ARISING IN ANY WAY OUT OF THE USE *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.**/
    /* USER CODE BEGIN (0) *//* USER CODE END */
    /* Include Files */
    #include "sys_common.h"#include "system.h"
    /* USER CODE BEGIN (1) */#include "can.h"#include "esm.h"#include "sys_core.h"
    #define D_COUNT  8 
    uint32 cnt=0, error =0, tx_done =0;uint8 tx_data[D_COUNT][8] = {0};uint8 rx_data[D_COUNT][8] = {0};uint8 *tx_ptr = &tx_data[0][0];uint8 *rx_ptr = &rx_data[0][0];uint8 *dptr=0;
    void dumpSomeData();/* USER CODE END */

    /** @fn void main(void)*   @brief Application main function**/
    /* USER CODE BEGIN (2) *//* USER CODE END */

    void main(void){/* USER CODE BEGIN (3) */
        /* enable irq interrupt in Cortex R4 */    _enable_interrupt_();
        /** - writing a random data in RAM - to transmit */    dumpSomeData();            /** - configuring CAN1 MB1,Msg ID-1 to transmit and CAN2 MB1 to receive */    canInit();
        /** - enabling error interrupts */        canEnableErrorNotification(canREG1); canEnableErrorNotification(canREG2);        /** - starting transmission */     for(cnt=0;cnt<D_COUNT;cnt++)    {               canTransmit(canREG1, canMESSAGE_BOX1, tx_ptr); /* transmitting 8 different chunks 1 by 1 */      while(tx_done == 0){};                 /* ... wait until transmit request is through        */      tx_done=0;      tx_ptr +=8;    /* next chunk ...*/    }        /** - check the received data with the one that was transmitted */    tx_ptr = &tx_data[0][0];    rx_ptr = &rx_data[0][0];            for(cnt=0;cnt<63;cnt++)     {          if(*tx_ptr++ != *rx_ptr++)          {               error++; /* data error */          }     }
        while(1){}; /* wait forever after tx-rx complete. */ /* USER CODE END */ }
    /* USER CODE BEGIN (4) *//* writing some data to ram  */void dumpSomeData(){     uint32 tmp = 0x11;          cnt = (D_COUNT*8)-1;     dptr = &tx_data[0][0];     *dptr = tmp;
         while(cnt--)     {        tmp = *dptr++;        *dptr = tmp + 0x11;     }}

    /* can interrupt notification *//* Note-You need to remove canMessageNotification from notification.c to avoid redefinition */void canMessageNotification(canBASE_t *node, uint32 messageBox){     /* node 1 - transfer request */     if(node==canREG1)      {            tx_done=1; /* confirm transfer request */     }
         /* node 2 - receive complete */          if(node==canREG2)     {      while(!canIsRxMessageArrived(canREG2, canMESSAGE_BOX1));      canGetData(canREG2, canMESSAGE_BOX1, rx_ptr); /* copy to RAM */          rx_ptr +=8;          }     
        /* Note: since only message box 1 is used on both nodes we dont check it here.*/}/* USER CODE END */

  • 好的,谢谢您慷慨的帮忙