This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我用F021的函数写内部flash可以,写EE就不能写进去了,为什么



uint32_t Fapi_BlockProgram( uint32_t Bank, uint32_t Flash_Address, uint32_t Data_Address, uint32_t SizeInBytes)
{
    register uint32_t src = Data_Address;
    register uint32_t dst = Flash_Address;
    uint32_t bytes;

    if (SizeInBytes < 16)
        bytes = SizeInBytes;
    else
        bytes = 16;

    if ((Fapi_initializeFlashBanks((uint32_t)SYS_CLK_FREQ)) == Fapi_Status_Success)
    {
         (void)Fapi_setActiveFlashBank(Fapi_FlashBank7);
         if(Bank >= 7)
             Fapi_enableEepromBankSectors(0xffffffff, 0xffffffff);
         else
             (void)Fapi_enableMainBankSectors(0xFFFF);                    /* used for API 2.01*/
    }else
    {
         return (1);
    }

    while( FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady );
    while( FAPI_GET_FSM_STATUS != Fapi_Status_Success );

    while( SizeInBytes > 0)
    {
        Fapi_issueProgrammingCommand((uint32_t *)dst,
                                     (uint8_t *)src,
                                     (uint32_t) bytes,
                                     0,
                                     0,
                                     Fapi_AutoEccGeneration);

         while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy );
        while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);

        src += bytes;
        dst += bytes;
        SizeInBytes -= bytes;
        if ( SizeInBytes < 16){
           bytes = SizeInBytes;
        }
    }
    return (0);
}
这是写扇区的函数,有的时候可以写进去,有的时候卡在第二个while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);这里,一直循环