This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f149的串口通信

利用usart0,通过rs232,与pc通信,接收pc发送的命令,只有一个字符时,可以正常接收,当多个字符时,接收出错,有相关例子可供参考一下吗?谢谢

  •   串口每次只能接收并处理一个字符。如果有多个字符,处理方法是开个缓存,全部接收下来再慢慢处理。以下代码供参考

    #include "include.h"
    
    void Uart_Init()//串口初始化  9600波特率 8-N-1
    {
    	U0CTL |= CHAR;//UART Mode,8-bits,1 stop bit,no parity
    	U0TCTL |= SSEL0;//Source select-ACLK
    	//波特率计算9600
    	U0BR1 = 0x00;
    	U0BR0 = 0x03;
    	U0MCTL = 0x4A;
    	UCTL0 &= ~SWRST;// Initialize USART state machine
    	ME1 |= UTXE0 + URXE0;//使能串口发送和接收
    	IE1 |= URXIE0;//开启串口接收中断使能
    	P3SEL |= BIT4 + BIT5;//开启IO口第二功能(作为串口收发端)
    }
    
    /*串口接收中断子程序*/
    #pragma vector = USART0RX_VECTOR
    __interrupt void UART_RX()
    {
    	_DINT();
            unsigned char tp_rx;
    	tp_rx = U0RXBUF; 
    	if(!rx_finish)//如果一帧没接收完,继续接收
    	{
    		if(rx_enable)//如果接收允许
    		{                       
    			buf_gps[count_gps] = tp_rx; //接收 
    			if(count_gps==4) get_gpsmode(); //接收到5个数据的时候,check mode	
    			if(tp_rx=='*'){ rx_enable = 0; rx_finish = 1;} //接收到'*'的时候,一帧结束
    			else count_gps++;             
    		}
    		else
    		{                          
    			if(tp_rx=='$'){ rx_enable = 1; count_gps = 0; rmc_gga = 0;}//如果接收到的字符是'$',则表示一帧的开始,使能串口接收
    		}
    	}
    	if(tp_rx=='#') upload_enable = 1; //收到'#',准备上传记录
            _EINT();
    }
    
    void UART_TX(uchar tp_tx)
    {	
    	IE1 &= ~URXIE0;//关闭串口接收中断使能
    	U0TXBUF = tp_tx;//发送数据				
    	while((IFG1 & UTXIFG0)==0);//等待发送完成
    	IE1 |= URXIE0;//开启串口接收中断使能
    }
    
  • 参考TI MSPWARE例程先跑通UART功能,跑通例程后在调试和PC通信。

  • 接收一个或几个字符后,如果有复杂的操作,可能影响到了串口的时序。建议采用2楼的方法