Other Parts Discussed in Thread: MSP430F249
如何设置相关寄存器?有例程吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
//******************************************************************************
// MSP430x24x Demo - USCI_B0 I2C Master RX single bytes from MSP430 Slave
//
// Description: This demo connects two MSP430's via the I2C bus. The master
// reads from the slave. This is the master code. The data from the slave
// transmitter begins at 0 and increments with each transfer. The received
// data is in R5 and is checked for validity. If the received data is
// incorrect, the CPU is trapped and the P1.0 LED will stay on. The USCI_B0
// RX interrupt is used to know when new data has been received.
// ACLK = n/a, MCLK = SMCLK = BRCLK = default DCO = ~1.045Mhz
//
// /|\ /|\
// MSP430F249 10k 10k MSP430F249
// slave | | master
// ----------------- | | -----------------
// -|XIN P3.1/UCB0SDA|<-|---+->|P3.1/UCB0SDA XIN|-
// | | | | | 32kHz
// -|XOUT | | | XOUT|-
// | P3.2/UCB0SCL|<-+----->|P3.2/UCB0SCL |
// | | | P1.0|--> LED
//
// B. Nisarga
// Texas Instruments Inc.
// September 2007
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.42A
//******************************************************************************
#include "msp430x24x.h"
unsigned char RXData;
unsigned char RXCompare;
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P1OUT &= ~0x01; // P1.0 = 0
P1DIR |= 0x01; // P1.0 output
P3SEL |= 0x06; // Assign I2C pins to USCI_B0
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC; // I2C Master, synchronous mode
UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
UCB0BR0 = 12; // fSCL = SMCLK/12 = ~100kHz
UCB0BR1 = 0;
UCB0I2CSA = 0x048; // Slave Address is 048h
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
IE2 |= UCB0RXIE; // Enable RX interrupt
RXCompare = 0x0; // Used to check incoming data
while (1)
{
while (UCB0CTL1 & UCTXSTP); // Ensure stop condition got sent
UCB0CTL1 |= UCTXSTT; // I2C start condition
while (UCB0CTL1 & UCTXSTT); // Start condition sent?
UCB0CTL1 |= UCTXSTP; // I2C stop condition
__bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts
if (RXData != RXCompare) // Trap CPU if wrong
{
P1OUT |= 0x01; // P1.0 = 1
while (1); // Trap CPU
}
RXCompare++; // Increment correct RX value
}
}
// USCI_B0 Data ISR
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
{
RXData = UCB0RXBUF; // Get RX data
__bic_SR_register_on_exit(CPUOFF); // Exit LPM0
}
//******************************************************************************
// MSP430x24x Demo - USCI_B0 I2C Slave TX single bytes to MSP430 Master
//
// Description: This demo connects two MSP430's via the I2C bus. The master
// reads from the slave. This is the slave code. The TX data begins at 0
// and is incremented each time it is sent. An incoming start condition
// is used as a trigger to increment the outgoing data. The master checks the
// data it receives for validity. If it is incorrect, it stops communicating
// and the P1.0 LED will stay on. The USCI_B0 TX interrupt is used to know
// when to TX.
// ACLK = n/a, MCLK = SMCLK = default DCO = ~1.045Mhz
//
// /|\ /|\
// MSP430F249 10k 10k MSP430F249
// slave | | master
// ----------------- | | -----------------
// -|XIN P3.1/UCB0SDA|<-|---+->|P3.1/UCB0SDA XIN|-
// | | | | |
// -|XOUT | | | XOUT|-
// | P3.2/UCB0SCL|<-+----->|P3.2/UCB0SCL |
// | | | |
//
// B. Nisarga
// Texas Instruments Inc.
// September 2007
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.42A
//******************************************************************************
#include "msp430x24x.h"
unsigned char TXData;
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P3SEL |= 0x06; // Assign I2C pins to USCI_B0
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMODE_3 + UCSYNC; // I2C Slave, synchronous mode
UCB0I2COA = 0x48; // Own Address is 048h
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
UCB0I2CIE |= UCSTTIE; // Enable Start condition interrupt
IE2 |= UCB0TXIE; // Enable TX interrupt
TXData = 0xff; // Used to hold TX data
while (1)
{
__bis_SR_register(CPUOFF + GIE); // Enter LPM0 w/ interrupts
}
}
// USCI_B0 Data ISR
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
{
UCB0TXBUF = TXData; // TX data
__bic_SR_register_on_exit(CPUOFF); // Exit LPM0
}
// USCI_B0 State ISR
#pragma vector = USCIAB0RX_VECTOR
__interrupt void USCIAB0RX_ISR(void)
{
UCB0STAT &= ~UCSTTIFG; // Clear start condition int flag
TXData++; // Increment data
}