Other Parts Discussed in Thread: MSP430F4250, MSP430F4270
MSP430F4250的A2通道是差分输入ADC通道,被分配到P1.7,P1.6端口,我想使用A2通道应该怎么配置呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F4250, MSP430F4270
MSP430F4250的A2通道是差分输入ADC通道,被分配到P1.7,P1.6端口,我想使用A2通道应该怎么配置呢?
和使用其他通道基本是一样的
下面是一个使用通道5的例程
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//*****************************************************************************
// MSP430x42x0 Demo - SD16_A, Using the Integrated Battery Sensor
//
// Description: This example shows how to use the SD16_A module's integrated
// Battery sensor (connected to input channel 5) to measure VCC.
// A single conversion is initiated and then the CPU is disabled by entering
// LPM0. Once the conversion has completed, a SD16_A interrupt occurs and
// stores the result in variable "ADCresult". LED lights if batter is low
// ACLK = LFXT1 = 32768 Hz, MCLK = SMCLK = DCO = 32 x ACLK = 1048576 Hz
// //* An external watch crystal on XIN XOUT is required for ACLK *//
// //* Minimum Vcc is required for SD16_A module - see datasheet *//
// //* 100nF cap btw Vref and AVss is recommended when using 1.2V ref *//
//
// MSP430F4270
// -----------------
// /|\| XIN|-
// | | | 32kHz
// --|RST XOUT|-
// | |
// |A5+ | ( A5+, A5- connected internally )
// |A5- |
// | |
// | VREF |---+
// | | |
// | | -+- 100nF
// | | -+-
// | | |
// | AVss |---+
// | |
//
// L. Westlund / S. Karthikeyan
// Texas Instruments Inc.
// June 2005
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.30A
//*****************************************************************************
#include <msp430.h>
#define LOW_BAT 0xBFFF // ~3V
static unsigned int ADCresult;
int main(void)
{
volatile unsigned int i; // Use volatile to prevent removal
// by compiler optimization
P1DIR |= 0x01;
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
FLL_CTL0 |= XCAP14PF; // Configure load caps
for (i = 0; i < 10000; i++); // Delay for 32 kHz crystal to
// stabilize
SD16CTL = SD16REFON+SD16SSEL0; // 1.2V ref, SMCLK
SD16CCTL0 |= SD16SNGL+SD16IE ; // Single conv, enable interrupt
SD16INCTL0 |= SD16INCH_5; // Select Channel A5
for (i = 0; i < 0x3600; i++); // Delay for 1.2V ref startup
__enable_interrupt(); // Enable general interrupts
while (1)
{
SD16CCTL0 |= SD16SC; // Set bit to start conversion
__bis_SR_register(LPM0_bits); // Enter LPM0
if( ADCresult < LOW_BAT )
{
P1OUT |= 0x01;
}
else
{
P1OUT &= ~0x01;
}
__no_operation(); //SET BREAKPOINT HERE
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=SD16_VECTOR
__interrupt void SD16ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(SD16_VECTOR))) SD16ISR (void)
#else
#error Compiler not supported!
#endif
{
switch (SD16IV)
{
case 2: // SD16MEM Overflow
break;
case 4: // SD16MEM0 IFG
ADCresult = SD16MEM0; // Save results (clears IFG)
break;
}
__bic_SR_register_on_exit(LPM0_bits); // Exit LPM0
}
dongwei fu 说:谢谢您的程序,不过我已经找到问题的所在了,虽然说都是AD转换通道,但是对于MSP430F4250来说,它的AD通道的配置不全是一样的
是的 4250的是 16位 高精度 Sigma Delta ADC