Other Parts Discussed in Thread: MSP430F5244
如何计算MSP430F5244 的IIC的UCB0BR0和UCB0BR1的值?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5244
如何计算MSP430F5244 的IIC的UCB0BR0和UCB0BR1的值?
The I2C clock SCL is provided by the master on the I2C bus. When the USCI is in master mode, BITCLK is
provided by the USCI bit clock generator and the clock source is selected with the UCSSELx bits. In slave
mode, the bit clock generator is not used and the UCSSELx bits are don't care.
The 16-bit value of UCBRx in registers UCBxBR1 and UCBxBR0 is the division factor of the USCI clock
source, BRCLK. The maximum bit clock that can be used in single master mode is fBRCLK/4. In multi-master
mode, the maximum bit clock is fBRCLK/8. The BITCLK frequency is given by:
fBitClock = fBRCLK/UCBRx
参见TI用户手册中说明