Other Parts Discussed in Thread: ADS1115, MSP430G2231
有用msp430调过ads1115驱动模块吗,能发一份资料吗,一直调不出来
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以参考下下面这段:
这是写8bit的,修改成data有16bit即可。
//******************************************************************************
// MSP430F20xx Demo - I2C Master Receiver, single byte
//
// Description: I2C Master communicates with I2C Slave using
// the USI. Slave data should increment from 0x00 with each transmitted byte
// which is verified by the Master.
// LED off for address or data Ack; LED on for address or data NAck.
// ACLK = n/a, MCLK = SMCLK = Calibrated 1MHz
//
// ***THIS IS THE MASTER CODE***
//
// Slave Master
// (msp430x20x3_usi_09.c)
// MSP430F20x2/3 MSP430F20x2/3
// ----------------- -----------------
// /|\| XIN|- /|\| XIN|-
// | | | | | |
// --|RST XOUT|- --|RST XOUT|-
// | | | |
// LED <-|P1.0 | | |
// | | | P1.0|-> LED
// | SDA/P1.7|------->|P1.7/SDA |
// | SCL/P1.6|<-------|P1.6/SCL |
//
// Note: internal pull-ups are used in this example for SDA & SCL
//
// Z. Albus
// Texas Instruments Inc.
// May 2006
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A
//******************************************************************************
#include <msp430g2231.h>
#define DELAY_START_CYCLES 20
//void i2c_usi_mst_wait_usi_cnt_flag();
void FORCING_SDA_HIGH(void)
{
USISRL = 0xFF;
USICTL0 |= USIGE;
USICTL0 &= ~(USIGE+USIOE);
}
void FORCING_SDA_LOW(void)
{
USISRL = 0x00;
USICTL0 |= USIGE+USIOE;
USICTL0 &= ~USIGE;
}
void DELAY(int delay)
{
int i;
for (i = 0; i < delay; i++);
}
////////////////////////////////////////////////////////////////////////////////////////////
char addr = 0xC0; // Address is 0x48 << 1 bit + 0 for Write
char reg = 0x08;
char data = 0xA0; // Variable for received data
char RW;
int i =0;
void I2Cwrite(char,char,char);
void I2Cread(char, char);
int I2C_State = 0; // State variable
// function to generate I2C REPEATED START condition
void i2c_usi_mst_gen_repeated_start(void)
{
USICTL0 |= USIOE;
USISRL = 0xFF;
USICNT = 1;
// wait for USIIFG is set
//i2c_usi_mst_wait_usi_cnt_flag();
// small delay
//DELAY(DELAY_START_CYCLES);
DELAY(50);
// pull down SDA to create START condition
FORCING_SDA_LOW();
// small delay
//DELAY(DELAY_START_CYCLES);
}
void main(void)
{
volatile unsigned int i; // Use volatile to prevent removal
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog
if (CALBC1_1MHZ ==0xFF || CALDCO_1MHZ == 0xFF)
{
while(1); // If calibration constants are erased
// do not load, trap CPU!!
}
BCSCTL1 = CALBC1_1MHZ; // Set DCO
DCOCTL = CALDCO_1MHZ;
P1OUT = 0xC0; // P1.6 & P1.7 Pullups
P1REN |= 0xC0; // P1.6 & P1.7 Pullups
P1DIR = 0xFF; // Unused pins as outputs
P2OUT = 0;
P2DIR = 0xFF;
USICTL0 = USIPE6+USIPE7+USIMST+USISWRST;// Port & USI mode setup
USICTL1 = USII2C+USIIE; // Enable I2C mode & USI interrupt
USICKCTL = USIDIV_7+USISSEL_2+USICKPL;// Setup USI clocks: SCL = SMCLK/8 (~120kHz)
USICNT |= USIIFGCC; // Disable automatic clear control
USICTL0 &= ~USISWRST; // Enable USI
USICTL1 &= ~USIIFG; // Clear pending flag
_EINT();
//I2Cwrite(0xc0, 0x08, 0x90);
//I2Cwrite(0xc0, 0x10, 0x90);
//I2Cwrite(0xc0, 0x07, 0xB0);
//I2Cwrite(0x90, 0x01, 0xaa);
while(1)
{
I2Cwrite(0xc0, 0x03, 0xe8);
//I2Cwrite(0xc0, 0x10, 0x90);
//I2Cwrite(0xb0, 0x03, 0xc5);
// I2Cread(0xc0, 0x08);
// I2Cread(0xc0, 0x10);
// I2Cread(0xc0, 0x07);
// I2Cread(0x90, 0x04);
// I2Cread(0x90, 0x05);
I2Cread(0xb0, 0x03);
I2Cread(0xc0, 0x03);
}
}
/******************************************************
// USI interrupt service routine
******************************************************/
#pragma vector = USI_VECTOR
__interrupt void USI_TXRX (void)
{
switch(I2C_State)
{
case 0: // Generate Start Condition & send address to slave
P1OUT |= 0x01; // LED on: sequence start
USISRL = 0x00; // Generate Start Condition...
USICTL0 |= USIGE+USIOE;
USICTL0 &= ~USIGE;
USISRL = addr; // ... and transmit address, R/W = 1
USICNT = 0x08; // Bit counter = 8, TX Address
I2C_State = 2; // Go to next state: receive address (N)Ack
break;
case 2: // Receive Address Ack/Nack bit
USICTL0 &= ~USIOE; // SDA = input
USICNT |= 0x01; // Bit counter = 1, receive (N)Ack bit
I2C_State = 4; // Go to next state: check (N)Ack
break;
case 4: // Send Reg
USICTL0 |= USIOE; // SDA = output
USISRL = reg;
USICNT |= 0x08; // Bit counter = 8, RX data
I2C_State = 5; // Go to next state: Test data and (N)Ack
break;
case 5: // Receive Reg Ack/Nack bit
USICTL0 &= ~USIOE; // SDA = input
USICNT |= 0x01; // Bit counter = 1, receive (N)Ack bit
if(RW==0)
I2C_State = 6; // Go to next state: send data
else
I2C_State = 7;
break;
case 6: // Send Data
USICTL0 |= USIOE; // SDA = output
USISRL = data; // ... and transmit address, R/W = 1
USICNT = 0x08; // Bit counter = 8, TX Address
I2C_State = 10; // Go to next state: receive address (N)Ack
break;
case 7: // Generate Start Condition & send address to slave
i2c_usi_mst_gen_repeated_start();
// USISRL = 0x00; // Generate Start Condition...
// USICTL0 |= USIGE+USIOE;
// USICTL0 &= ~USIGE;
//USICTL0 |= USIOE; // SDA = Output
USISRL = addr|0x01; // ... and transmit address, R/W = 1
USICNT = 0x08; // Bit counter = 8, TX Address
I2C_State = 8; // Go to next state: receive address (N)Ack
break;
case 8:
USICTL0 &= ~USIOE; // SDA = input
USICNT |= 0x01; // Bit counter = 1, receive (N)Ack bit
I2C_State = 9;
break;
case 9: //Read only Read back
USICTL0 &= ~USIOE; // SDA = input
USICNT |= 0x08; // Bit counter =8 Reg read back
USICTL0 |= USIOE; // SDA = Output
USISRL = 0xff;
USICNT |= 0x01; // Bit counter =8 Reg read back
I2C_State = 11;
break;
case 10: // Receive Data Ack/Nack bit
USICTL0 &= ~USIOE; // SDA = input
USICNT |= 0x01; // Bit counter = 1, receive (N)Ack bit
I2C_State = 11;
break;
case 11: // Prep Stop Condition
USICTL0 |= USIOE; // SDA = output
USISRL = 0x00;
USICNT |= 0x01; // Bit counter = 1, SCL high, SDA low
I2C_State = 12; // Go to next state: generate Stop
break;
case 12: // Generate Stop Condition
USISRL = 0x0FF; // USISRL = 1 to release SDA
USICTL0 |= USIGE; // Transparent latch enabled
USICTL0 &= ~(USIGE+USIOE);// Latch/SDA output disabled
I2C_State = 0; // Reset state machine for next transmission
break;
}
USICTL1 &= ~USIIFG; // Clear pending flag
}
void I2Cwrite(char addr1, char reg1, char data1)
{
addr=addr1, reg=reg1, data=data1;
RW=0;
USICTL1 |= USIIFG; // Set flag and start communication
for (i = 0; i < 500; i++);
}
void I2Cread(char addr1, char reg1)
{
addr=addr1, reg=reg1;
//RW bit =1
RW=1;
USICTL1 |= USIIFG; // Set flag and start communication
for (i = 0; i < 500; i++);
}