Other Parts Discussed in Thread: ADC124S021
在配置4线SPI时STE引脚功能需要配置成 P1SEL |=BIT4
P1SEL2 |=BIT4 吗?
下图没怎么看懂,配置UCMODE模式后,UCxSTE的输出状态怎么改变???是用P1OUT改变输出状态吗?(以P1.4为例)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADC124S021
在配置4线SPI时STE引脚功能需要配置成 P1SEL |=BIT4
P1SEL2 |=BIT4 吗?
下图没怎么看懂,配置UCMODE模式后,UCxSTE的输出状态怎么改变???是用P1OUT改变输出状态吗?(以P1.4为例)
您好,还有个问题需要请教一下。最近用launchpadG2和ADC124S021及串口做一个采集电压采集系统,通过串口发送ADC采集的数据到PC端,用IO口模拟SPI通信就没有问题,但是采样速率不快(大约为9k)所以想提高采样速率,就想用硬件4线SPI提高采样速率。ADC采集一次数据然后把数据发送到PC端,在数据发送过程中,ADC需要关闭吗即把STE引脚拉高?????ADC输出数据为16位实际只有12位有效,SPI接收寄存器只能接收8位,需要接收两次然后再发,对吧?SPI主控模式能不能硬件仿真?我用IAR在线仿真,观看RXBUF的值,一直有变化,理论上应该只有第二次的数据会有变化(低八位)。