Other Parts Discussed in Thread: ADC124S021, MSP430G2553
用G2553作为控制芯片,用IO口模拟SPI与ADC124S021通信时,再通过串口发送数据,没有问题。但是用硬件SPI时,串口发送数据一直是0000,示波器上能够看到ADC有数据输出,(串口程序没有问题,可单独运行),请问正确采集到发送的顺序是什么?这个问题困扰了几天,希望大神指教一下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADC124S021, MSP430G2553
用G2553作为控制芯片,用IO口模拟SPI与ADC124S021通信时,再通过串口发送数据,没有问题。但是用硬件SPI时,串口发送数据一直是0000,示波器上能够看到ADC有数据输出,(串口程序没有问题,可单独运行),请问正确采集到发送的顺序是什么?这个问题困扰了几天,希望大神指教一下,谢谢
程序如下,如果格式不好看,可以看附加中main.c文件
#include "MSP430G2553.h"
unsigned int get_H=0,get_L=0,AD_V=0;
float result=0;
int i;
int floag=0;
unsigned char table[5];
void uart_init(void);
void send_dat(unsigned char ch);
void spi_init(void);
void main( void )
{
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
DCOCTL = CALDCO_12MHZ;
BCSCTL1 = CALBC1_12MHZ;
uart_init();
spi_init();
__enable_interrupt(); //打开总中断
while(1)
{
if(floag == 1) //判断是否读取了16位数据
{
floag = 0; //标志位清零
result = ((get_H & 0X0F)*256 + get_L)*3.3/4095 ; //ADC为12位,高四位无效,参考电压3.3V
AD_V = (int)(result * 1000);
table[0]=AD_V/1000 + '0';
table[1]=AD_V%1000/100 + '0';
table[2]=AD_V%100/10 + '0';
table[3]=AD_V%10 + '0';
table[4]=' ';
for(i=0;i<5;i++)
send_dat(table[i]);
P1OUT &=~BIT4;
}
}
}
//------------串口初始化-------------------
void uart_init(void)
{
P1SEL |= BIT1 +BIT2;
P1SEL2 |= BIT1 + BIT2;
UCA0CTL1 |=UCSSEL_2;
UCA0BR0 =0XE2;
UCA0BR1 = 0X04; //时钟12MHZ,波特率9600
UCA0MCTL = 0X00;
UCA0CTL1 &=~ UCSWRST;
}
//------------发送数据--------------------
void send_dat(unsigned char ch)
{
while(!(IFG2 & UCA0TXIFG)); //等待发送完成
UCA0TXBUF = ch;
}
//-------------SPI初始化---------------------------
/* ADC引脚
* P1.4 STE 1 CS
* P1.5 CLK 10 CLK
* P1.6 SOMI 9 DOUT
* P1.7 SIMO 8 DIN
* 本次用到3线SPI,4线SPI的STE引脚不会配置
***************************************************/
void spi_init(void)
{
P1DIR |= BIT4; //从器件选择端
P1SEL |= BIT5 + BIT6 + BIT7;
P1SEL2 |= BIT5 + BIT6 + BIT7;
UCB0CTL1 = UCSWRST;
UCB0CTL0 |= UCMSB + UCMST + UCSYNC; //高位优先,主控,3线,同步时钟,CLK选择模式0
UCB0CTL1 |= UCSSEL_2; //时钟源选择SMCLK
UCB0BR0 = 15; //SPI时钟0.8M,12M/0.8M=15
UCB0BR1 = 0X00;
UCB0CTL1 &=~UCSWRST; //启动SPI
UCB0TXBUF = 0X18; //0X18为ADC的控制命令,选择通道4
P1OUT &=~ BIT4 ; //选通ADC
}
#pragma vector=USCIAB0TX_VECTOR
__interrupt void UCB0TX_DAT(void)
{
UCB0TXBUF = 0X18;
}
#pragma vector=USCIAB0RX_VECTOR
__interrupt void UCB0RX_DAT(void)
{
i++;
if(i==1)
{
get_H = UCB0TXBUF; //i=1读取高8位
}
else
{
i=0;
get_L = UCB0TXBUF; //i=2读取低8位
floag =1; //用来标志,spi已经读取了16位数据
P1OUT |= BIT4; //拉高CS
}
}