Other Parts Discussed in Thread: MSP430FR2311
Hi,
我用MSP430FR2311 输出pwm,TB0输出pwm正常;由于pcb板子已经步好了,只能用TB1.2(P2.1),但是不能输出pwm,code如下所示:
#include "driverlib.h"
#define TIMER_PERIOD 511
#define DUTY_CYCLE 383
void main(void)
{
//Stop WDT 2k、364、481
WDT_A_hold(WDT_A_BASE);
//P1.6 as PWM output
GPIO_setAsPeripheralModuleFunctionOutputPin(
GPIO_PORT_P2,
GPIO_PIN1,
GPIO_SECONDARY_MODULE_FUNCTION
);
//Disable the GPIO power-on default high-impedance mode to activate
//previously configured port settings
PMM_unlockLPM5();
//Generate PWM - Timer runs in Up mode
Timer_B_outputPWMParam param = {0};
param.clockSource = TIMER_B_CLOCKSOURCE_SMCLK;
param.clockSourceDivider = TIMER_B_CLOCKSOURCE_DIVIDER_1;
param.timerPeriod = TIMER_PERIOD;
param.compareRegister = TIMER_B_CAPTURECOMPARE_REGISTER_2;
param.compareOutputMode = TIMER_B_OUTPUTMODE_RESET_SET;
param.dutyCycle = DUTY_CYCLE;
Timer_B_outputPWM(TIMER_B1_BASE, ¶m);
//Enter LPM0
__bis_SR_register(LPM0_bits);
//For debugger
__no_operation();
}
谢谢!