Other Parts Discussed in Thread: MSP430L092, MSP-FET
大神们好,最近需要使用MSP430L092这款芯片,各种找资料发现比较少,用的人也不多。然后买了5片芯片(买都很难买的到)。现在遇到下载问题,查了官方的资料,说MSP-TS430L092这个可以是吗? 求大家解说下,是不是只能用这款下载器(因为我查了下,这个下载器超级贵),所以求大神们帮忙看看。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430L092, MSP-FET
大神们好,最近需要使用MSP430L092这款芯片,各种找资料发现比较少,用的人也不多。然后买了5片芯片(买都很难买的到)。现在遇到下载问题,查了官方的资料,说MSP-TS430L092这个可以是吗? 求大家解说下,是不是只能用这款下载器(因为我查了下,这个下载器超级贵),所以求大神们帮忙看看。
2-1:需要一个MSP430下载调试器
MSP430L092必须使用标准JTAG(4线制)下载,不支持SBW(2线制JTAG)。
所以要选择支持4线JTAG方式的下载器。建议使用 MSP-FET430UIF 或MSP-FET,
购买链接如下:https://store.ti.com/msp-fet.aspx
想了解更多MSP430的调试工具,可参考以下文档:
中文文档zhcu019l:http://www.ti.com.cn/cn/lit/ug/zhcu019l/zhcu019l.pdf
(第13页有个表格,里边列出了支持4线JTAG的调试工具。英文版里有更新的工具)
英文文档slau278y:http://www.ti.com/lit/ug/slau278y/slau278y.pdf
2-2:还需要电平转换电路板
假设你已经有调试器,例如MSP-FET430UIF,还不能直接使用。
MSP430L092支持超低工作电压:0.9V to 1.5 V (1MHz);1.5V to 1.65V (4 MHz);
需要通过一个转接板将MSP-FET430UIF上的电源电压和JTAG信号(1.8-3.6V)降为适用于MSP430L092电路板的电压。
其实几个电平转换芯片,原理图等可以参考以下网页:
http://www.ti.com.cn/tool/cn/MSP-TS430L092
关于这个型号的更多资源,可参考下边帖子:
http://www.deyisupport.com/blog/b/msp430/archive/2014/02/14/0-9v-msp430l092-mcu.aspx?
另外,芯片购买的话,可以直接到TI Store购买的: