This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6736 UCS的疑问

用6736做了一块板子,在进行UCS的初始化时,运行初始化代码如下:

UCSCTL6 &= ~(XT1OFF);                   // Enable XT1

   UCSCTL6 |= XCAP_1;                      // Internal load cap

   // Loop until XT1, XT2 & DCO fault flag is cleared

   do

   {

       UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG);

       // Clear XT2,XT1,DCO fault flags

       SFRIFG1 &= ~OFIFG;                  // Clear fault flags

       //for(unsigned int i=0;i<50000;i++);

   }

   while (SFRIFG1 & OFIFG);              // Test oscillator fault flag

PJDIR |= BIT0 | BIT1 | BIT3;           // ACLK, MCLK, SMCLK set out to pins

   PJSEL |= BIT0 | BIT1 | BIT3;           // PJ.0,1,3 for debugging purposes.

虽然能够从while( SFRIFG1 & OFIFG )里面跳出来,可是OFIFG的值仍然是1,同时DCOFFG的值也是1,从PJ.3管脚也看不到32k的波形。换了好几个晶振了仍然不行,请问这是为什么,OFIFG置位了自检还能通过?同时我看到了UG上说,DCO=0或者31时DCOFFG会置位,可是DCO的值似乎不是用户软件可以设置的啊,请大神赐教啊!

补充一条,在单步运行时,运行完了SFRIFG1 &= ~OFIFG; 这一句之后,UCSCTL0寄存器会变成0x00F8也就是DCO的值变成了0。DCOFFG为1,XT1LFOFFG和XT2OFFG为0。