This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2755 硬件I2C MCU RESET



G2755做I2C从机,在测试中发现,主机低频率(每条数据间隔100MS读取)读取数据正常,而高频率(每条数据间隔10MS)读取数据时会出现概率性MCU自动复位现象。

  • I2C速率设的多少?

  • 主从机都是100KHZ。如下:初始化配置和中断处理。

    void TI_USCI_I2C_slaveinit(void (*SCallback)(),
    void (*TCallback)(unsigned char volatile *value),
    void (*RCallback)(unsigned char value),
    void (*StCallback)(),
    unsigned char slave_address){
    P3SEL |= SDA_PIN + SCL_PIN; // Assign I2C pins to USCI_B0
    UCB0CTL1 |= UCSWRST; // Enable SW reset
    UCB0CTL0 = UCMODE_3 + UCSYNC; // I2C Slave, synchronous mode
    UCB0CTL1 = UCSSEL_2 + UCSWRST; // Use SMCLK, keep SW reset
    UCB0BR0 = 10; // Set prescaler 1M/10~100KHZ
    UCB0BR1 = 0;
    UCB0I2COA = slave_address; // set own (slave) address
    UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
    IE2 |= UCB0TXIE + UCB0RXIE; // Enable TX RX interrupt
    UCB0I2CIE |= UCSTTIE+UCSTPIE; // Enable STT STP interrupt
    TI_start_callback = SCallback;
    TI_stop_callback = StCallback;
    TI_receive_callback = RCallback;
    TI_transmit_callback = TCallback;
    }

    #pragma vector = USCIAB0TX_VECTOR
    __interrupt void USCIAB0TX_ISR(void)
    {
    if (IFG2 & UCB0TXIFG)
    {
    TI_transmit_callback(&UCB0TXBUF);
    }
    else
    {
    TI_receive_callback(UCB0RXBUF);
    }

    }

    // USCI_B0 State ISR
    #pragma vector = USCIAB0RX_VECTOR
    __interrupt void USCIAB0RX_ISR(void)
    {
    if(UCB0STAT&UCSTTIFG)
    {
    UCB0STAT &= ~UCSTTIFG; // Clear start condition int flag
    rxnum=0;//接收到开始信号清零
    }
    if(UCB0STAT&UCSTPIFG)
    {
    UCB0STAT&=~UCSTPIFG;
    TI_stop_callback();
    }
    }

  • 通讯造成复位的常见原因主要有以下三种:

    1、非法操作了某个寄存器;

    2、数据溢出

    3、通讯时序错误,等待到看门狗超时

    楼主看看最可能是遇到了哪一种