This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP430FR2111 内置温度传感器校准值的问题

Other Parts Discussed in Thread: MSP430FR2111

Dear All,

我们公司目前有生产过一批产品,使用的是MSP430FR2111,有使用了该MCU内置的温度传感器,但是在使用过程中发现使用内置的ADC去读取温度传感器的值,再根据CALADC_15V_85C和CALADC_15V_30C来计算温度值,在室温为27度的情况下,测出来的值普遍偏高,500台里有几十台读数超过36度的,有一台读值为2度,误差达到了25度,更换MCU后工作正常。按理来说,这个校准值应当是TI校准过的才对,使用官方提供的示例程序测试,结果一样。所以我们想问一下大家有没有遇到过类似的问题,谢谢大家

  • 没遇到过。我用过的msp430内置温度传感器误差都在手册提供的误差范围内。

  • 关于MSP430 内置温度传感器的精度,有如下说明

    产品说明书中提供了带有相应容差范围的额定 00C 电压与温度系数。额定 00C 电压规定为986mV,其最大误差为 +/- 5%。因此,温度传感器的 00C 电压在最恶劣的环境下,每个器件可能会相差几乎 +/- 50mV。这大约等于 +/- 14C。请注意,这种差异主要与各个器件有关,因此,只要对单个器件进行适当校准,即可通过满分辨率的 ADC12 获得非常准确的绝对温度。