Other Parts Discussed in Thread: MSP430FG4618
小弟这几天在测试MSP430驱动LCD的功耗测试,手里有的MSP430FG4618的测试板,板上只有两个晶振32768Hz和30MHz,还有就是基本上电复位电路,测试使用库的标准例子。以下是测试的结程序和结果:
1:当按照上面的程序进行测试里,LCD屏接与不接,电流都在0.1~0.2uA;
2:当把程序中的休眠模式改成LPM3时,不接LCD屏电流40~45uA,接上LCD屏电流50~60uA;
3:如果把程序中LCDA初始化部分去除,同样在LPM3模式下,测试板电流2.5uA左右;
请问各位高手,LCDA的工作电流真的这么大吗?这好像手册中说只要3uA?如何进一点减小功耗呢?
PS:所用LCD屏为3.3V 4mux + 3bias的笔段屏
谢谢啦!