应用MSP430F417方案做了一个小的系统,碰到偶尔程序死掉的情况,此时量测32.768Khz的晶振没有起来,比较奇怪的是量测RESET#信号的电平只有1.8V左右,正常情况此信号的电平为3.1V,RESET电路为1M电阻与0.1uF电容做的RC电路,RESET#信号只连到MCU与一个芯片上;如果重新插拔一下电源,此现象消失系统可以正常工作,RESET#也变为3.1V;如果有描述不清楚地方,请随时提出,谢谢.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应用MSP430F417方案做了一个小的系统,碰到偶尔程序死掉的情况,此时量测32.768Khz的晶振没有起来,比较奇怪的是量测RESET#信号的电平只有1.8V左右,正常情况此信号的电平为3.1V,RESET电路为1M电阻与0.1uF电容做的RC电路,RESET#信号只连到MCU与一个芯片上;如果重新插拔一下电源,此现象消失系统可以正常工作,RESET#也变为3.1V;如果有描述不清楚地方,请随时提出,谢谢.
问题已经查明,RST#信号用万用表和灵敏高的示波器测量为3.1v,属于正常情况.而用小型示波器测量为1.8V;
估计是因为上拉电阻为1M电流太小导致小型示波器测量时出现误差.程序死掉的问题还是存在,正在Debug;
谢谢!