This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC700EVM UART RX端短接到地



Hi,

我使用TDC1000-TDC7200EVM , 用GPIO3\GPIO4 (对应uart端的tx、rx)和其他板子通信,在测试时将gpio3、4短接,可以正常通信,可是过了一段时间之后,发现不能通信,tx可以正常发送,可rx始终无法收到数据,如果rx和tx短接,示波器中tx端也没有数据信号,感觉好像是rx端短接到地了。

这个开发板其它的测量功能仍然正常。

我该怎么做?需要再买一块板子吗?还是有可以解决的办法?