This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs9.1添加头文件问题

Other Parts Discussed in Thread: MSP430FR6989

当我在使用ccs9.1添加头文件时总是出现各种各样的问题,例如在创建一个名为LCDTEST新工程时,为它中添加 OutOfBox_MSP430FR6989例程中的hal_LCD.c与hal_LCD.h时编译总会出现各种问题,但如果把main.c中的代码放到 OutOfBox_MSP430FR6989例程当中就不会出现问题。我想要知道应该如何为一个新工程添加头文件,我已经尝试过http://processors.wiki.ti.com/index.php/Include_paths_and_options中的方法,仍然行不通,请尽可能完整的演示一下应该如何为一个新工厂添加头文件,谢谢

  • 根据您的描述,应该还是路径的问题。我会实验一下后给您回复
  • 以下是我的测试结果,可以成功编译

    新建了工程名为6989的工程

    步骤如下

    1 新建工程

    2 右键点击工程名,选择Properties,在include option 内添加了driverlib的路径 (C:\ti\msp\MSP430Ware_3_80_07_00\driverlib\driverlib\MSP430FR5xx_6xx)

    3 右键点击工程名,选择Add Files,将hal_LCD.c和hal_LCD.h都link到工程,如下图

    4 完成上述步骤后编译就可以了

  • 感谢您的回答,但我仍然行不通,以下为错误信息
    **** Build of configuration Debug for project 6989 ****

    "D:\\ti\\ccs\\utils\\bin\\gmake" -k -j 8 all -O

    Building file: "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c"
    Invoking: MSP430 Compiler
    "D:/ti/ccs/tools/compiler/ti-cgt-msp430_18.12.2.LTS/bin/cl430" -vmspx --data_model=restricted --use_hw_mpy=F5 --include_path="D:/ti/ccs/ccs_base/msp430/include" --include_path="D:/ti/msp430_driverlib_2_91_11_01/driverlib/MSP430FR5xx_6xx" --include_path="C:/Users/ewang/Desktop/program/tiworkspace/6989" --include_path="C:/Users/ewang/Desktop/driver of r6989/lcd" --include_path="D:/ti/ccs/tools/compiler/ti-cgt-msp430_18.12.2.LTS/include" --advice:power=all --advice:hw_config=all --define=__MSP430FR6989__ --define=_MPU_ENABLE -g --printf_support=minimal --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --preproc_with_compile --preproc_dependency="driver of hal_LCD.d_raw" "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c"

    >> Compilation failure
    subdir_rules.mk:9: recipe for target 'hal_LCD.obj' failed
    "C:\Users\ewang\Desktop\driver of r6989\lcd\hal_LCD.h", line 44: warning #41-D: expected an identifier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 99: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 100: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 101: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 102: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 103: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 146: error #20: identifier "mode" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 165: warning #225-D: function "showChar" declared implicitly
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 165: error #20: identifier "pos1" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 166: error #20: identifier "pos2" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 167: error #20: identifier "pos3" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 168: error #20: identifier "pos4" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 169: error #20: identifier "pos5" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 170: error #20: identifier "pos6" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 150: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 155: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 156: remark #2553-D: (ULP 14.1) Array index (involving "t") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 158: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #2553-D: (ULP 14.1) Array index (involving "j") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 172: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 155: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 156: remark #2553-D: (ULP 14.1) Array index (involving "t") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 158: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #2553-D: (ULP 14.1) Array index (involving "j") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 172: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 180: warning #161-D: declaration is incompatible with previous "showChar" (declared at line 165)
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 185: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 186: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 191: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 191: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 192: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 192: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 197: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 197: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 198: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 198: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 203: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 204: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 213: error #20: identifier "pos1" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 215: error #20: identifier "pos2" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 217: error #20: identifier "pos3" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 219: error #20: identifier "pos4" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 221: error #20: identifier "pos5" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 223: error #20: identifier "pos6" is undefined
    13 errors detected in the compilation of "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c".
    gmake: *** [hal_LCD.obj] Error 1
    Building file: "../main.c"
    Invoking: MSP430 Compiler
    "D:/ti/ccs/tools/compiler/ti-cgt-msp430_18.12.2.LTS/bin/cl430" -vmspx --data_model=restricted --use_hw_mpy=F5 --include_path="D:/ti/ccs/ccs_base/msp430/include" --include_path="D:/ti/msp430_driverlib_2_91_11_01/driverlib/MSP430FR5xx_6xx" --include_path="C:/Users/ewang/Desktop/program/tiworkspace/6989" --include_path="C:/Users/ewang/Desktop/driver of r6989/lcd" --include_path="D:/ti/ccs/tools/compiler/ti-cgt-msp430_18.12.2.LTS/include" --advice:power=all --advice:hw_config=all --define=__MSP430FR6989__ --define=_MPU_ENABLE -g --printf_support=minimal --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"
    Finished building: "../main.c"

    gmake: Target 'all' not remade because of errors.

    **** Build Finished ****

  • 请将CCS和MSP430WARE都放在默认路径,您这样是很容易出问题
  • 我已将CCS和MSP430WARE重新安装于默认路径,仍然不行

  • 与之前的错误相同,控制台错误信息为:
    **** Build of configuration Debug for project 6989 ****

    "C:\\ti\\ccs910\\ccs\\utils\\bin\\gmake" -k -j 8 all -O

    Building file: "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c"
    Invoking: MSP430 Compiler
    "C:/ti/ccs910/ccs/tools/compiler/ti-cgt-msp430_18.12.2.LTS/bin/cl430" -vmspx --data_model=restricted --use_hw_mpy=F5 --include_path="C:/ti/ccs910/ccs/ccs_base/msp430/include" --include_path="C:/ti/msp/MSP430Ware_3_80_07_00/driverlib/driverlib/MSP430FR5xx_6xx" --include_path="C:/Users/ewang/Desktop/program/tiworkspace/6989" --include_path="C:/Users/ewang/Desktop/driver of r6989/lcd" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-msp430_18.12.2.LTS/include" --advice:power="all" --advice:hw_config=all --define=__MSP430FR6989__ --define=_MPU_ENABLE -g --printf_support=minimal --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --preproc_with_compile --preproc_dependency="driver of hal_LCD.d_raw" "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c"

    >> Compilation failure
    subdir_rules.mk:9: recipe for target 'hal_LCD.obj' failed
    "C:\Users\ewang\Desktop\driver of r6989\lcd\hal_LCD.h", line 44: warning #41-D: expected an identifier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 99: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 100: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 101: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 102: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 103: remark #1546-D: (ULP 15.1) Detected consecutive bitfield assigns. Recommend using bit mask instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 146: error #20: identifier "mode" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 165: warning #225-D: function "showChar" declared implicitly
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 165: error #20: identifier "pos1" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 166: error #20: identifier "pos2" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 167: error #20: identifier "pos3" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 168: error #20: identifier "pos4" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 169: error #20: identifier "pos5" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 170: error #20: identifier "pos6" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 150: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 155: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 156: remark #2553-D: (ULP 14.1) Array index (involving "t") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 158: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #2553-D: (ULP 14.1) Array index (involving "j") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 172: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 155: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 156: remark #2553-D: (ULP 14.1) Array index (involving "t") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 158: remark #1544-D: (ULP 13.1) Detected loop counting up. Recommend loops count down as detecting zeros is easier
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #1545-D: (ULP 14.1) Array index of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 161: remark #2553-D: (ULP 14.1) Array index (involving "j") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 172: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 180: warning #161-D: declaration is incompatible with previous "showChar" (declared at line 165)
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 185: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 186: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 191: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 191: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 192: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 192: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 197: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 197: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 198: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 198: remark #2553-D: (ULP 14.1) Array index (involving "c") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 203: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 204: remark #2553-D: (ULP 14.1) Array index (involving "position") of type "int". Recommend using "unsigned int"
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 213: error #20: identifier "pos1" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 215: error #20: identifier "pos2" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 217: error #20: identifier "pos3" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 219: error #20: identifier "pos4" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 221: error #20: identifier "pos5" is undefined
    "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c", line 223: error #20: identifier "pos6" is undefined
    13 errors detected in the compilation of "C:/Users/ewang/Desktop/driver of r6989/lcd/hal_LCD.c".
    gmake: *** [hal_LCD.obj] Error 1
    gmake: Target 'all' not remade because of errors.

    **** Build Finished ****
  • 这个问题是编译器没有找到相应的文件,是典型的工程配置问题。

    "C:\Users\ewang\Desktop\driver of r6989\lcd\hal_LCD.h", line 44: warning #41-D: expected an identifier

    添加这个目录的时候,把反斜杠改为正斜杠试试