我现使用MSP430AFE253单片机来做一个数据采集电路。查看文档得知该单片机的24位AD非高阻抗输入,因此在输入端使用运放做了个电压跟随器,通过实验发现使用德仪的LM358是可以的。用上脚对脚的TLC2272和其他品牌的358后测量数据跳动非常大,但是拿高精万用表测试跟随输出端却很稳定。现排除运放质量问题,因为在别的电路使用没有问题。几百个数加权滤波也不行。供电采用+5v和-1.5V供电,应该也没有问题,现在怀疑单片机ADC的输入是不是对运放某个参数有特殊要求?跟随输入如图很简单
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现使用MSP430AFE253单片机来做一个数据采集电路。查看文档得知该单片机的24位AD非高阻抗输入,因此在输入端使用运放做了个电压跟随器,通过实验发现使用德仪的LM358是可以的。用上脚对脚的TLC2272和其他品牌的358后测量数据跳动非常大,但是拿高精万用表测试跟随输出端却很稳定。现排除运放质量问题,因为在别的电路使用没有问题。几百个数加权滤波也不行。供电采用+5v和-1.5V供电,应该也没有问题,现在怀疑单片机ADC的输入是不是对运放某个参数有特殊要求?跟随输入如图很简单