我使用的芯片是MSP430F2131,我查看芯片手册,发现该芯片没有XT2时钟源,而使用高频时钟只能采用DCOCLK。
我需要一个12M的时钟源,但是出厂的DCOCLK精度达不到我们的要求,因此我们需要对DCOCLK校准,然而主时钟也得用DCOCLK,所以好像达不到预期的效果,请问这种情况我们还可以采取什么手段来校准DCO时钟呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用的芯片是MSP430F2131,我查看芯片手册,发现该芯片没有XT2时钟源,而使用高频时钟只能采用DCOCLK。
我需要一个12M的时钟源,但是出厂的DCOCLK精度达不到我们的要求,因此我们需要对DCOCLK校准,然而主时钟也得用DCOCLK,所以好像达不到预期的效果,请问这种情况我们还可以采取什么手段来校准DCO时钟呢
关于DCO精度的问题,你一般需要考虑两个因素,一个是芯片的工作电压,一个是工作温度。
一般说DCO的精度,都会考虑在全温度范围,还是室温,工作电压时可变的,还是固定的某一个具体的电压值。
MSP430F2131的DCO的精度,可以参考datasheet的23页,里面很详细的说明了在室温下,全温下,不同工作电压下的温度。
https://www.ti.com.cn/cn/lit/ds/symlink/msp430f2131.pdf
关于校准参数,我们提供了相关的程序
http://dev.ti.com/tirex/explore/node?node=AFBWDiHlS1d3fquUBkb3LQ__IOGqZri__LATEST
//****************************************************************************** // MSP430F21x2 Demo - DCO Calibration Constants Programmer // // NOTE: THIS CODE REPLACES THE TI FACTORY-PROGRAMMED DCO CALIBRATION // CONSTANTS LOCATED IN INFOA WITH NEW VALUES. USE ONLY IF THE ORIGINAL // CONSTANTS ACCIDENTALLY GOT CORRUPTED OR ERASED. // // Description: This code re-programs the F2xx DCO calibration constants. // A software FLL mechanism is used to set the DCO based on an external // 32kHz reference clock. After each calibration, the values from the // clock system are read out and stored in a temporary variable. The final // frequency the DCO is set to is 1MHz, and this frequency is also used // during Flash programming of the constants. The program end is indicated // by the blinking LED. // ACLK = LFXT1/8 = 32768/8, MCLK = SMCLK = target DCO // //* External watch crystal installed on XIN XOUT is required for ACLK *// // // MSP430F21x2 // --------------- // /|\| XIN|- // | | | 32kHz // --|RST XOUT|- // | | // | P1.0|--> LED // | P2.1|--> SMLCK = target DCO // // A. Dannenberg // Texas Instruments Inc. // December 2007 // Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A //******************************************************************************
另外我们提供了