Part Number: MSP430FR5724
下图是MSP430FR5724低功耗电流值,按照表格给出的数据,芯片工作频率在1MHz和8MHz的LPM0低功耗模式下电流值差别不大,这样理解是否正确
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR5724
下图是MSP430FR5724低功耗电流值,按照表格给出的数据,芯片工作频率在1MHz和8MHz的LPM0低功耗模式下电流值差别不大,这样理解是否正确
芯片工作频率在1MHz和8MHz的LPM0低功耗模式下电流值差别不大,这样理解是否正确
该测试是有一定的条件的,如
All inputs are tied to 0 V or to VCC. Outputs do not source or sink any current
从图表来看,(特定测试条件下)芯片工作频率在8MHz的LPM0低功耗模式下电流值比1MHz大一些
为了使MSP430最大限度的达到低功耗,对于MSP430未使用的GPIO而言,应该将其设置为输出;或者是设置为输入,但是将管脚的电平固定,可以通过外部电路将管脚连接至Vcc或者GND,也可使能内部上下拉电阻,将管脚电平固定。
您可以看一下