Part Number: MSP430FR5724
您好,请问430在仿真调试的时候进入低功耗后寄存器界面的CCSTEP能不能用来作程序运行时间的参照
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
430在仿真调试的时候进入低功耗
在连接仿真器在CCS调试时,芯片是在LPM0的,您现在是想测试哪个低功耗状态?
程序运行时间的话,您可以使用clock工具
https://e2echina.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/200001/faq-ccs
您好,测试的低功耗状态是LPM3,我使用的软件是IAR,运行的程序为MSP430FR57xx_LPM3_02.c,调试界面窗口如下
您可以使用CYCLECOUNTER。记录延时函数前后的CYCLECOUNTER值,差值就是程序运行的时钟周期
时钟频率乘以时钟周期就可以计算出时间了
您好,请问一下在实际的调试中,遇到LPM3低功耗程序时CYCLECOUNTER好像不能反映真实的时间。MSP430FR57xx_LPM3_02.c程序看门狗定时1s,主系统时钟频率是4Mhz,左图是开始调试前,右图是运行到中断。请问一下这是什么原因。