Part Number: MSP430F2419

图所示为项目中MSP430F4219的初始化配置(XT2=8MHz),其中注释部分(P6)在调试时异常。
现象:
1、该段代码注释后系统正常运行;加入该段代码,系统无法完成管脚初始化配置;
2、将未注释的代码下载到另一个项目的板子(XT2=6MHz)上,管脚能正常初始化配置。
请教下大家,出现这种问题的原因以及解决的办法。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F2419

图所示为项目中MSP430F4219的初始化配置(XT2=8MHz),其中注释部分(P6)在调试时异常。
现象:
1、该段代码注释后系统正常运行;加入该段代码,系统无法完成管脚初始化配置;
2、将未注释的代码下载到另一个项目的板子(XT2=6MHz)上,管脚能正常初始化配置。
请教下大家,出现这种问题的原因以及解决的办法。谢谢!
q请问是否有直接测试TI例程?您现在测试的有问题的板子,P6的功能是什么?
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430x26x Demo - Basic Clock, MCLK Configured to Operate from XT2 HF XTAL
//
// Description: Proper selection of an external HF XTAL for MCLK is shown
// using HF XT2 OSC. OFIFG is polled until the HF XTAL is stable; only then is
// MCLK sourced by XT2. MCLK is buffered on P5.4 and MCLK/10 is on P1.1 driven
// by a software loop taking exactly 10 CPU cycles.
// ACLK = MCLK = LFXT1 = HF XTAL, SMCLK = default DCO ~1.045MHz
// //* XT2 HF XTAL NOT INSTALLED ON FET *//
// //* Min Vcc required varies with MCLK frequency - refer to datasheet *//
//
// MSP430F261x/241x
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// | |
// | XT2IN|-
// | | HF XTAL (400kHz - 16MHz)
// | XT2OUT|-
// | |
// | P1.1|-->MCLK/10 = XT2 HFXTAL/10
// | P5.4/MCLK|-->MCLK = XT2 HFXTAL
//
// B. Nisarga
// Texas Instruments Inc.
// September 2007
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.42A
//******************************************************************************
#include <msp430.h>
volatile unsigned int i;
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P5DIR |= 0x10; // P5.4= output direction
P5SEL |= 0x10; // P5.4= MCLK option select
P1DIR |= 0x02; // P1.1 = output direction
BCSCTL1 &= ~XT2OFF; // Activate XT2 high freq xtal
BCSCTL3 |= XT2S_2; // 3 � 16MHz crystal or resonator
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFF; i > 0; i--); // Time for flag to set
}
while (IFG1 & OFIFG); // OSCFault flag still set?
BCSCTL2 |= SELM_2; // MCLK = XT2 HF XTAL (safe)
for (;;) // Infinite loop
{
P1OUT |= 0x02; // P1.1 = 1
P1OUT &= ~0x02; // P1.1 = 0
}
}
不是TI的例程。P6.1、P6.6为普通IO输出配置,P6.4、P6.7为ADC输入配置。
ADC12SSEL=MCLK=8MHz,ADC12DIV=1/4。
另外我试了一下,将P6全配置为输出也是同样的问题。

P6.6是P6.4 ADC检测模块的电源控制键,常关状态。现先将P6.6配置,使ADC检测模块正常工作,再配置P6.4为ADC输入,程序运行正常。配置如下:

刚才问题使解决了,但是好像不是根本原因。现在配置换了下也能正常运行了。

再初始化配置的时候其实两种表达效果是一样的。而且之前这样设置也是没有问题。例如下图的代码段就能正常运行。

不知道最根本的原因是啥。为了避免以后出问题,还是按照OK的那种方式来配置。
谢谢您的反馈
a |= b就是将a,b 做按位”或“运算,结果给a,相当于a = a | b;