Part Number: MSP430FR5724
请问一下在MSP430FR57xx_adc10_11.c中,有以下两个问题
1.概述部分上面写的是ADC采样周期为16Hz,但是按产生的脉冲信号ACLK/1024,上升沿触发采样,应该是32Hz
2.下面写到了有32ms的开启周期,请问这个时间是如何计算出来的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR5724
请问一下在MSP430FR57xx_adc10_11.c中,有以下两个问题
1.概述部分上面写的是ADC采样周期为16Hz,但是按产生的脉冲信号ACLK/1024,上升沿触发采样,应该是32Hz
2.下面写到了有32ms的开启周期,请问这个时间是如何计算出来的
这个例程触发ADC使用的是TimerA0的输出模式4翻转模式,在计数值等于CCR1处翻转,所以输出周期是设定周期(CCR0)的两倍:

(slau272d_MSP430FR57xx Family User's Guide (Rev. D)Table 11-2. Output Modes)

(Figure 11-12. Output Example – Timer in Up Mode)
括号中的注释可能造成了误解,但是程序没有问题。