This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F149单片机 捕获外部中断 后怎么一直在中断函数中循环

问题如标题,外部中断是接收到红外信号

#include <msp430x14x.h>
#define uchar unsigned char
#define uint unsigned int
uint temp,temp1;
long start, end, time ;

void delay(void)
  {
    uint f=500;
    while(f--);
  }


void delayms(int ms)
{
  while(ms--)
  { 
    int i=0;
    for(i=0;i<=1600;i++);
  }
}


void init(void)
  { uint i;
   // P1DIR =0XFF 1OUT =0XFF;
    P2DIR =0XFF 2OUT =0XF0;
    P3DIR =0XFF 3OUT =0XFF;
    P4DIR =0XFF 4OUT =0XFF;
    P5DIR =0XFF 5OUT =0XFF;
    P6DIR =0XFF 6OUT =0XFF;
   
  
    
    P1DIR &=~BIT5;//P1IE = BIT5;
   // P1IES=BIT5; P1IFG =0X00;
    P1DIR &=~BIT2  1SEL =BIT2;
    _EINT();
    BCSCTL1 &=~XT2OFF;
    BCSCTL2 |= SELM1+DIVM_3;                
    TACTL=TASSEL_2+TACLR+MC_1 ; //timera_clk=Mclk=1MHz、连续计数模式、1分频
    CCTL1=CM_3+SCS+CCIS_0+CAP+CCIE;       
  
    
    
   do
    { 
      IFG1 &=~OFIFG;
       for(i=0xFF;i>0;i--);
    }
   while ((IFG1 & OFIFG)!=0);

    temp = temp1 = 0 ;
    start = end = time =0 ;
  }

void main(void)
  {
    WDTCTL =WDTPW+WDTHOLD ;
   init();
    uint i=0,j=0;
    
    while(1)
    {
     delayms(5);
         
     CCTL1 |=CCIE;
  
  
    }
  }

/********************Timer_A中断服务程序*************************/
#pragma vector = TIMERA1_VECTOR
__interrupt void Timer_A (void)
  {
   CCTL1 &=~CCIE;// TACTL |= MC_0;
   
    
    P2OUT ^=0xff;
    
    
  }