Other Parts Discussed in Thread: MSP430F249
原来是用的MSP430F249,后来空间不够了改用F2416,但是地址》0xFFFF的高位空间,不知道如果去擦写这些高位空间。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F249
原来是用的MSP430F249,后来空间不够了改用F2416,但是地址》0xFFFF的高位空间,不知道如果去擦写这些高位空间。
这部分内容在用户手册312页:http://www.ti.com/cn/lit/pdf/slau144,可以结合以下网页一起看:http://bbs.ednchina.com/BLOG_ARTICLE_2053410.HTM
谢谢Viki,但是网页中只有正常的对地位地址空间的读写方式。
如果我要对0x13000这个地址的扇区进行擦写操作的话,总是不成功。
void Test_WriteFlash(void)
{
U16 i;
char* pdb;
WDTCTL = WDTPW + WDTHOLD;
//second segment
pdb = (int *)FLASH_TEST;
FCTL3 = FWKEY; //clear lock bit
FCTL1 = FWKEY + ERASE; //set erase bit
*pdb = 0;
FCTL1 = FWKEY + WRT; //dummy write
while ((FCTL3 & BUSY) > 0);
*pdb = 0x55;
//-- disable flash write
FCTL1 = FWKEY;
FCTL3 = FWKEY + LOCK;
}
当#define FLASH_TEST 0x2000时,能够把0x2000地址的扇区删除并对第一个 字节写入0x55.
当#define FLASH_TEST 0x13000时,对0x13000地址的操作则无法成功。
总之就是, 当操作的FALSH地址超过了64KBYTE时,需要在编译器选项中处理器设置里将DATA/CODE MODE设置为LARGE。
上面是IAR中的操作,IAR 开发环境中,右键点项目名称进入Options for node "xxx", 在General Options的Target页面的Data Model选项中 选择Large模式.
为了防止别人也有类似问题,在CCS中时,操作如下:
希望对你有帮助!O(∩_∩)O~
BR,
Lina