This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5438A外部晶振XT1 (32768Hz)不起振

Other Parts Discussed in Thread: MSP430F6436

5438A配置:XT1:32K; XT2:12M;XT2起振,XT1无法起振。

编译器:IAR 5.3。

两块PCB板,第一块没有问题;第二块xt1不起振。换过晶振,换过mcu都不行,一直在循环中,XT1LFOFFG 一直为1;

void sysClock_Init(void)
{

P7SEL |= BIT0 + BIT1;                        /* Port select XT1*/
P5SEL |= BIT2 + BIT3;                         /* Port select XT2*/

UCSCTL6 |= XCAP_3;                          /* Internal load cap*/

UCSCTL6 &= ~(XT1OFF + XT2OFF); /* Set XT1 & XT2 On*/

/* Loop until XT1,XT2 & DCO stabilizes*/
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG);/* Clear XT2,XT1,DCO fault flags*/
SFRIFG1 &= ~OFIFG;                                                                               /* Clear fault flags*/
delay_us(50);                                                                                             /* Delay for Osc. to stabilize*/
}
while (SFRIFG1 & OFIFG);                                                                       /* Test oscillator fault flag*/

/* expected frequency*/
UCSCTL4 = SELS_5 + SELM_5; /* SMCLK=MCLK=XT2 ACLK=XT1*/
}