Other Parts Discussed in Thread: MSP430F417
最近在用msp430F417做个段码LCD显示的东西,屏为4mux,1/3bias,3.3V的,折腾了近半个月了,外部分压电阻的电压为屏的驱动偏置电压,结果外置电阻的分压总是不对,如0V,1.3V,1.7V,3.2V,应该为0V,1.1V,2.2V,3.3V,而且R13和R23的端口电压总有wave出现,求各位指导下,电路图和初始化程序如下
int main( void )
{
//close watchdog
WDTCTL = WDTPW + WDTHOLD;
//system clock set
FLL_CTL0 |= XCAP14PF; // Set load capacitance for xtal
SCFQCTL = 0x7f;
//LCD Controller register initial
LCDCTL = 0x3D; //001 S0-S15 are LCD function;11 4-mux;1 All LCD segments are enabled;unused;1 LCD timing generator and Ron are on
BTCTL = BTFRFQ0; // Set freqLCD = ACLK/64 = 512
// Set Rxx and COM pins for LCD
P5SEL = 0XFC;
//Port initial
P1DIR = 0x02; // P1.1 to output direction
P1SEL = 0x02; // P1.1 to output MCLK
P2DIR = 0XFF;
...............
}
谢谢大家。