Other Parts Discussed in Thread: MSP430F449
产品构成 MCU:MSP430F449 晶振:32.768K 有外部时钟芯片
晶振电路:外部晶振引脚各接了12PF的电容 程序中也配置:XCAP18PF
软软件:IAR 5.3
问题大概如下:MCU每隔500ms去读取时钟芯片的时间。根据时间去记录事件。假如我设置30秒这一刻记录一次事件。运行一段时间后,读取出来的记录事件丢失了。有些时刻记录不到。
我们在高温(60度)老化中出现的以上问题
开始我们以为是晶振问题,但是我们采用更好质量的晶振也是一样会出现。经过一段时间的实验和老化,发现将外部晶振引脚上的12PF电容去掉,就不会出现这种问题。
疑问:
1、MSP430的内部配置电容和外部电容是什么关系:并联吗
2、关于内部电容的配置以哪个为准,IAR的头文件是XCAP18PF写着是18pf 但是430的数据手册写着最大~10 pF
3、我们这样的配置会造成晶振停振或时钟失效么(内部配置XCAP18PF,外部12pf,晶振最佳负载电容12.5pf)。
44 4、MSP430F449的时钟管理系统有没办法解决这个问题,假设真的是外部的32K晶振停振,没有管理机制可以启用别的时钟源。