Other Parts Discussed in Thread: MSP430F5510
请问,为什么MSP430F5510的两个Uart口,串行通讯时候,波特率低于19200就可以,高于就出问题。
我的外设是57600,调试时候,MCU的TX发出数据OK,MCU RX到的数据就错误。
问题出现在哪里?其它的都检查了多遍。
设MCU设计的Bug 还是软件问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F5510
请问,为什么MSP430F5510的两个Uart口,串行通讯时候,波特率低于19200就可以,高于就出问题。
我的外设是57600,调试时候,MCU的TX发出数据OK,MCU RX到的数据就错误。
问题出现在哪里?其它的都检查了多遍。
设MCU设计的Bug 还是软件问题?
USCI31 USCI Module
Function: UART framing error after USCI software reset (UCSWRST)
Description: While receiving a byte over USCI-UART (with UCBUSY bit set), if the application resets
the USCI module (software reset via UCSWRST), then a framing error is reported for the
next receiving byte.
Workaround
• If possible, do not reset USCI-UART during an ongoing receive operation; that is,
when UCBUSY bit is set.
or
• If the application software resets the USCI module (via the UCSWRST bit) during an
ongoing receive operation, then set and reset the UCSYNC bit before releasing the
software USCI reset.
可以在errordata里查出来是否有uart上的bug。