Other Parts Discussed in Thread: MSP430F2011
我使用MSP-FET-430UIF烧录MSP430F2011芯片程序,然后我这个芯片什么电路都没搭,只是连接了下图,但是还是连接不了。程序错误原因是
Thu Oct 12, 2017 10:17:25: Could not initialize device interface
Thu Oct 12, 2017 10:17:26: Fatal error: Failed to initialize. Check if hardware is connected. Check if drivers are installed. Try to restart the computer. Tools using the parallel port are not supported on Windows Vista Session aborted!
Thu Oct 12, 2017 10:17:26: Failed to load debugee: E:\project\Debug\Exe\test.d43
请教各位大神怎么办!!!!