Other Parts Discussed in Thread: MSP430L092, MSP430FG4250, MSP430F4250
我需要一块既有ADC又有DAC的超低功耗芯片,差不多10位就可以了 然后电压是3.3V左右,芯片IO口也最好少点 引脚控制在20个以下,求大神推荐下,,,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430L092, MSP430FG4250, MSP430F4250
我需要一块既有ADC又有DAC的超低功耗芯片,差不多10位就可以了 然后电压是3.3V左右,芯片IO口也最好少点 引脚控制在20个以下,求大神推荐下,,,
Hi Chao Chen,
1. 既有ADC又有DAC,且IO在20以下的,可以看一下MSP430L092,但它的ADC和DAC位数为8位,工作电压为:
– 0.9 V to 1.5 V (1 MHz) – VOL Better Than 0.15 V at 2.5 mA
– 1.5 V to 1.65 V (4 MHz)
2. 既有ADC又有DAC,且在10位以上,电压为3.3V的,一般IO口会多一些,比如:MSP430F4250, MSP430FG4250等,你可以评估一下。
你的所有条件都满足的MCU应该没有。