This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询MSP432P4011处理器软复位指令

请问TI工程师:

      MSP432系列单片机 是否有 软复位指令  方便系统 主动复位用

  • /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2013, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     *
     *                       MSP432 CODE EXAMPLE DISCLAIMER
     *
     * MSP432 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/.../mspdriverlib for an API functional
     * library & https://dev.ti.com/pinmux/ for a GUI approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //   MSP432P401 Demo - Hard reset
    //
    //   Description: This code examples exercises the hard reset feature by
    //   triggering the hard reset with/out an assigned source number [0-15], and
    //   after reset the code checks for the source of the reset. The example cycles
    //   through hard reset w/o source and all hard reset sources, 0 to 15, and
    //   completes when all hard reset sources have been triggered and confirmed
    //   after subsequent resets.
    //
    //   Breakpoints can be set in each case statement to check when the associated
    //   hard reset was triggered/confirmed.
    //
    //   When you reach the very end of the code example, the device should have
    //   gone through 17 hard resets.
    //
    //  See msp432p401_reset_01 example for soft reset.
    //
    //                MSP432P401x
    //             -----------------
    //         /|\|                 |
    //          | |                 |
    //          --|RST              |
    //            |                 |
    //            |             P1.0|-->LED
    //
    //   Dung Dang
    //   Texas Instruments Inc.
    //   October 2015 (updated) | November 2013 (created)
    //   Built with Code Composer Studio V6.0
    //******************************************************************************
    #include "msp.h"
    #include "stdint.h"
    
    
    
    uint8_t* stateMachine = (uint8_t*)0x20005000;
    
    int main(void) {
        volatile uint32_t i;
    
        WDT_A->CTL = WDT_A_CTL_PW | WDT_A_CTL_HOLD;               // Stop WDT
        P1->DIR |= BIT0;                          // P1.0 set as output
        P1->OUT &= ~BIT0;                         // Turn off P1.0 LED
    
        /* Code test through hard resets with
            - No source
            - Source 0 -> 15in that order.
           After reset, check for source of reset to move on to next test
           After RSTCTL_HARDRESETSTAT_SRC15, all tests should pass
        */
    
    
        if (*stateMachine == 0x00)
        {
            /* stateMachine is the RAM variable that does not get re-initialized
             * after hard reset. */
            *stateMachine = 1;
    
            /* Issue hard reset without specified source */
            RSTCTL->RESET_REQ |= (0x6900 | RSTCTL_RESET_REQ_HARD_REQ);
        }
    
        /* Set breakpoints in the different case statements to check the source of
         * previous hard interrupt. Each breakpoint should only be hit once even
         * after resets.
         *
         * Remove all breakpoints to let the device run through all hard reset
         * iterations to the end of the code.
         */
    
        if (*stateMachine == 1)
        {
            switch (RSTCTL->HARDRESET_STAT)        // Get the source of the hard reset
            {
                case 0:                         // hard reset with no source indicated
                    /* Issue hard reset with source = 0 */
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC0;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC0:  // hard reset with source #0
                    /* Clear hard reset source by writing to reset clear register */
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC0;
                    /* Issue hard reset with the next source */
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC1;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC1:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC1;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC2;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC2:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC2;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC3;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC3:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC3;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC4;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC4:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC4;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC5;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC5:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC5;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC6;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC6:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC6;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC7;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC7:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC7;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC8;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC8:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC8;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC9;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC9:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC9;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC10;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC10:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC10;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC11;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC11:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC11;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC12;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC12:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC12;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC13;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC13:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC13;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC14;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC14:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC14;
                    RSTCTL->HARDRESET_SET |= RSTCTL_HARDRESET_SET_SRC15;
                    while(1);
                case RSTCTL_HARDRESET_STAT_SRC15:
                    RSTCTL->HARDRESET_CLR |= RSTCTL_HARDRESET_STAT_SRC15;
                    /* All hard reset sources have been exercised. Update stateMachine
                     * and conclude the example
                     */
                    *stateMachine = 2;
                    break;
    
                default:
                    while(1);
            }
    
        }
        /* *stateMachine == 2 means we've gone through all hard reset sources */
    
        if (*stateMachine == 2)
        {
            P1->OUT |= BIT0;                      // Turn on LED indicating success
    
            /* Reset the RAM variable *stateMachine to 0, in case you'd like to go
             * through the whole experience again by reseting the device */
            *stateMachine = 0;
        }
        else
        {
            while (1)
            {
                P1->OUT ^= BIT0;                  // Blink LED to indicate erroneous reset/execution in the code
                for (i=0;i<20000;i++);
            }
        }
    }