Part Number: TM4C123GH6PM
if(xQueueReceive(g_pLEDQueue, &i8Message, 0) == pdPASS)
{
//
// If left button, update to next LED.
//
if(i8Message == LEFT_BUTTON)
{
//
// Update the LED buffer to turn off the currently working.
//
g_pui32Colors[g_ui8ColorsIndx] = 0x0000;
//
// Update the index to next LED
g_ui8ColorsIndx++;
if(g_ui8ColorsIndx > 2)
{
g_ui8ColorsIndx = 0;
}
//
// Update the LED buffer to turn on the newly selected LED.
//
g_pui32Colors[g_ui8ColorsIndx] = 0x8000;
//
// Configure the new LED settings.
//
RGBColorSet(g_pui32Colors);
//
// Guard UART from concurrent access. Print the currently
// blinking LED.
//
xSemaphoreTake(g_pUARTSemaphore, portMAX_DELAY);
UARTprintf("Led %d is blinking. [R, G, B]\n", g_ui8ColorsIndx);
xSemaphoreGive(g_pUARTSemaphore);
}
//
// If right button, update delay time between toggles of led.
//
if(i8Message == RIGHT_BUTTON)
{
ui32LEDToggleDelay *= 2;
if(ui32LEDToggleDelay > 1000)
{
ui32LEDToggleDelay = LED_TOGGLE_DELAY / 2;
}
//
// Guard UART from concurrent access. Print the currently
// blinking frequency.
//
xSemaphoreTake(g_pUARTSemaphore, portMAX_DELAY);
UARTprintf("Led blinking frequency is %d ms.\n",
(ui32LEDToggleDelay * 2));
xSemaphoreGive(g_pUARTSemaphore);
}
}
//
// Turn on the LED.
//
RGBEnable();
//
// Wait for the required amount of time.
//
vTaskDelayUntil(&ui32WakeTime, ui32LEDToggleDelay / portTICK_RATE_MS);
//
// Turn off the LED.
//
RGBDisable();
//
// Wait for the required amount of time.
//
vTaskDelayUntil(&ui32WakeTime, ui32LEDToggleDelay / portTICK_RATE_MS);
}
}
这是上面freertos demo里的例程的led.c,看不懂,帮帮我吧,谢谢朋友们