This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843: 如何配置N2HET单元进行PWM输出与输入控制

Part Number: RM57L843


您好:

        我现在想使用N2HET单元,进行16路PWM输出,与8路PWM输入。参照HALGEN设计,N2HET的2个BANK中,采用相关封装好的API时,最多一次输出8路(可实时调整参数),也就是说2个BANK最多实现16路输出,但是8路采集也要求试试采集,又该如何实现。

      PS:HET_IDE生产的代码,无法实时更改参数,也不满足我的需求。

  • 但是8路采集也要求试试采集,又该如何实现。

    我个人建议是分时多路输出。用时间分割法,将 16 路 PWM 输出分割成两组,每组 8 路,并交替地在两个 BANK 中进行输出。每个 BANK 将负责 8 路 PWM 输出,然后您可以使用一个定时器或来控制两组输出的切换了