When I use uinflash to flash a program into TMS470MF03107,an error occurred with indication:
"Can't Run Target CPU: (Error -1268 @ 0x3090001) Device is locked up in Hard Fault or in NMI. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
CortexM3_0: File Loader: Memory write failed: Timed out waiting for target to halt while executing wr_pll.alg
CortexM3_0: GEL: File: E:\chenyuefeng\DATA_input\ABS\ABS_boot\ABS_boot2.6\Bootloader-can250k-V2.6.hex: Load failed."