inLx翻转模式下,给inHx和inLx相同的非100%占空比pwm波形,GHx输出一直为高电平,GLx正常输出翻转电压。请问该如何解决。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,很抱歉回复晚了。为了帮助您更好地解决该问题,能否提供以下信息:
1.只使用两相的是因为驱动的不是电机,是给一个类似电容的器件供电,所以只用两相来做一个全桥驱动电路。
这是完整的原理图。
2.SHA的电压在不接外部电路时约等于GVDD(12V)减去一个管压降,在接上外部电路之后,SHA的电压会随着外部电压变化。当电压值超过GVDD之后,SHA会固定在11V。
GHA的低电位输出似乎会被SHA的电位影响,随着SHA的增大,GHA的低电位会随着SHA增大 (如图)
当SHA增大到接近GVDD时,GHA就变成全高了。
GVDD至VBST的电压为GVDD减去管压降,即11.3V左右。
3.正在使用的FET是5N10-MS。