This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8871: DRV8871驱动电磁铁

Part Number: DRV8871
Other Parts Discussed in Thread: DRV8870, DRV8873, DRV8243-Q1

请教一下,DRV8871的输入端IN1、IN2输入的是静态数据,例如IN1=1(高电平)、IN2=0(低电平),持续时间为200ms,之后IN1=0,IN2=0,周期是2秒;测试发现,DRV8871的OUT1、OUT2输出为PWM波形,占空比为50%,持续时间是200ms(与IN1=1,IN2=0持续时间一直),请教一下,为什么OUT输出是PWM,而不是持续固定电平?

DRV8871的OUT1、OUT2连接的负载是双向保持式电磁铁(这个电磁铁可以正向加电、也可以反向加电;正向/反向加电时,电磁铁金属柱可以弹出/缩回),OUT1接电磁铁正极,OUT2接电磁铁负极。

通过搜集、查阅一些资料,告知DRV8871不能驱动螺线管,不知道是不是这个原因?

另外,麻烦推荐一款能驱动电磁铁(螺线管)的驱动器,供电+24V,OUT输出电流最好≥1.2A,驱动器输入端最好是电平控制(例如IN1、IN2),尽量不想用PWM控制,多谢!!!