This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
| Component | TI Part Number | Specs |
|---|---|---|
| MOSFET | CSD18532KCS | 100V, 70A, Rds(on)=4.9mΩ |
| Gate Driver | UCC27612 | 6A peak, 4ns propagation delay |
| Source Resistor | ZF12HT100JT50 | 0.01Ω, 1% tolerance |
| Thermal Pad | 5510-050-010 | 0.25°C·cm²/W, 0.5mm thickness |