This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL494: PSpice的TL494仿真占空比不变

Part Number: TL494


我在使用PSpice 23版本自带模型库中的TL494模型进行电流限制仿真时,使用1脚进行电流采样电阻电压采样,2脚采用电阻分压的方式进行限流值设置,仿真后,1脚电压大于2脚,但输出PWM波形的占空比并没有因此调节。之后,在我对4脚DTC脚电压分别从0VDC增加到0.5VDC、1VDC、2VDC、3VDC,在3VDC导致占空比为0,可以理解,但在3VDC以下时,最大占空比并没有因此自动调节,我现在不知道是不是PSpice 23自带库中TL494模型的问题,如果是PSpice 23版本的模型有问题,能否给我提供一下最新的TL494的Spice模型?

谢谢!