This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570: 如何实现多组不同电压电流的光伏板给同一个MPPT的最大化供电

Part Number: BQ25570


你好。

我采用BQ25570实现光伏板的充电,我有3组一样的光伏板,但是受到太阳光照射角度不一样,导致这3组光伏板的输出电流,输出电压不一样。

1,如何实现这3组光伏板的最大化能量输出到MPPT?比如光伏板1输出3V,光伏板2输出2.5V,光伏板3输出2V。

2,是否可以直接并联这3组光伏板,连接到MPPT?但是每组光伏板电压不一样,直接并联后电压是否会异常。

3,暂不考虑采用3片MPPT的方式。