Other Parts Discussed in Thread: REF2912, INA326
我的AD623工作在10V环境下,我用ref2912的输出1.25V做AD623的基准,但是,1.25被拉高到1.32左右 请问是怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
能否提供您的电路图。
或者您需要用比较精确的仪器来测试这个高精度电压,同时需要注意是否是GND的noise导致的,用示波器确认。
其次注意输入电压低于5.5V。
GND的noise应该不会这么大把?而且是稳定的ref2912,也就是说虽然被拉高了,但是拉高到了1.3V,还是稳定的,不是随便跳动的,输入电压不低于5.5V?您的意思是REF2912的输入电压么? 我的ref2912的输入电压只有3.3