Other Parts Discussed in Thread: BQ24170
我前后设计了2版PCB,一版是只有BQ24170及其组件,做成一个独立的锂电池充电器,没有问题;
另一版是放在电源管理的线路板中,前级是AD-DC输出14V的电源作为输入,经过锂电池充电这个模块,后级是DC-DC的稳压电源输出,分别输出12V、5V、3.3V。然后,问题就来了:在不接电池的情况下,发现5V、3.3V无法输出100mA以上的电流,超过就直接拉掉BQ24170这个模块的输入电压,使这个模块不工作,以致后面所有供电都出现问题。这时测量BQ24170的内部LDO输出引脚为2.6V,正常工作时为3.3V。但是如果是12V输出接负载,能输出1A的电流,也就是正常工作了。如果接上锂电池,那所有供电都正常了。
哪位大侠能帮我分析一下可能问题点。我能想到的是,初步认为是PCB布线的问题,但我仔细的检查了几条走大电流的主线,都是超过1.5mm线宽,实在找不出其它问题了。
请大家帮我看看