This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: CEDV建模过程中,记录温度问题

Part Number: BQ4050


        我有个问题,电池建模过程中,电池放到高低温柜中,设置好温度,电池放电过程中要比设置温度高。 

        例如常温重载、常温轻载   25℃  3A 重载  1A轻载 放电。

        我记录数据,上传建模 温度是一直是室温25,还是电芯再室温25℃真实温度?????

        因为电池放电会发热肯定会比25℃高,谁能帮我解答这个问题。