This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z110自学习怎么设置?

Other Parts Discussed in Thread: BQ34Z110

请问一下TI的工程师,校正完电流、电压几个参数后,怎么让BQ34Z110进入自学习状态和量产。

1.为什么电池多次充放电(按照0.2C),都未能进入学习状态,标志位也没有变化。

2.另外两个指令0x41复位,和0x0021使能,是用软件EVSW的I2C PRO里发送的吗?那为什么没有反应呢?

3.另外,外接NTC温度传感器,需要校正吗, 不校正测量的值准确不?另外能测量零下的温度吗?

  • 1. 首先Qmax cell 0 要先修改为和Design capacity一样, 再使能QEN,发送0021 之后,QEN会置位, Update Status 会变成04

    2. 再循环充放电,注意充电一定要使FC置位, 在等待2小时,等VOK由1变为0,  再开始放电。 放电截止后等待5 小时。

    3. 42 和21 命令可以在pro发送, 也可以在SBS DATA界面的Control中直接输入0041或0021,点确定。

    4. NTC如果选择的型号和TIEVM版上一样,10K AT103 可以直接用,不用校准, 如果不是参照,http://www.ti.com/lit/zip/sluc568 

    http://www.ti.com/lit/pdf/slua398