Part Number: TPS62A01

您好!在WEBENCH® POWER DESIGNER 看了下,没有推荐前馈电容。这个值是按规格书上的选120PF吗?
Input:
DC 3.4 V - 4.4 V
Output:
3.3 V at 0.1-0.5 A 是不是3.3V不需要这个前馈电容呢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS62A01

您好!在WEBENCH® POWER DESIGNER 看了下,没有推荐前馈电容。这个值是按规格书上的选120PF吗?